Total vehicle systems
Space is tight on construction sites, and there are people working everywhere. Contractors need powerful machines that can maneuver in a narrow spot and perform with maximum efficiency and safety. Danfoss is a strong partner for the total vehicle system.
Danfoss fluid conveyance solutions are integral in construction applications, ensuring efficient fluid transport crucial for heavy machinery and equipment operation. Our durable components and precise systems play a pivotal role in maintaining construction site productivity and operational reliability.
Whether preparing the ground, enabling building work or landscaping the area around a new building, construction equipment must meet the highest demands for performance. Precise maneuverability and robust work functions are a necessity – along with responsive, ergonomic controls for machine operators.
At Danfoss, we work with you to design the best hydraulic solution for your entire system. Using our broad toolbox of modular components and intelligent PLUS+1® software, sensors and controls, we deliver the transmission, steering, cooling and work functions that your machines need to get the job done.
Take the boom on a telehandler or the arm of an aerial lift for example. Accurate, smooth and safe operation is essential near buildings where people are working on scaffolding or in the lift basket. Our modular PVG valves combined with SIL2 sensors and PLUS+1® controls are made for that type of challenge.
Seamless system integration is one of the Danfoss hallmarks. We can also connect your entire fleet with Danfoss Telematics – our remote management solutions for construction equipment on the move.
Fueling construction precision with innovation and unmatched reliability
In the dynamic realm of construction, Danfoss fluid conveyance solutions stand tall as indispensable assets, ensuring seamless and reliable fluid management crucial for heavy machinery and site operations. These robust solutions, featuring top-grade hoses and fittings, serve as the backbone of efficient fluid transport within construction sites. By focusing on durability and performance, Danfoss fluid conveyance solutions bolster the reliability and productivity of construction operations, enabling seamless hydraulic and fluid systems pivotal for heavy equipment and machinery functionality.
Maximizing uptime and efficiency, Danfoss components and systems are engineered to withstand the rigors of construction environments, providing essential fluid handling capabilities necessary for smooth project execution. Through optimized fluid transport, cooling, and hydraulic systems, these solutions not only enhance equipment longevity but also streamline construction workflows, empowering construction firms to achieve higher productivity and efficiency.

Addressing your challenges
Your machines can help make the world a better place — and Danfoss engineers can use their systems knowledge and expertise to help make your machines strong competitors in the marketplace.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }MBS 1200 mobile hydraulic pressure transmitterMBS 1200 series is a dedicated pressure transmitter program for mobile hydraulic applications.
MBS 1200 is a compact pressure transmitter, and offers a reliable pressure measurement, even under harsh environmental conditions. -
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }DST P92S SIL2, PLd pressure transmitter for mobile hydraulicEnsure functional safety in mobile hydraulic machinery with DST P92S SIL2 pressure sensors. When SIL2 or PL d is required for safe work environments.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Position sensorsDanfoss is taking functional safety to the next level with a full program of state-of-the-art rotary position sensors, wire position sensors, and inclination sensors. All three sensor types come as both single and redundant sensor types, making the complete portfolio suitable for safety-critical applications.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }MBS 9200 milibar pressure transmitter for general purpose applicationsMBS 9200 is designed for use in general purpose applications where low pressure are measured in the milibar range.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Flexible temperature sensor, MBT 3270The flexible temperature sensor MBT 3270 can be used in many industrial and cooling applications such as: air compressors, hydraulics as well as cooling systems. In other words, applications where robustness, size, and performance matters.
Related applications
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Crane and material handlingCranes and other large handling machines are required to operate within very specific load ranges. Danfoss provides pressure transmitters that supply load limiting systems with crucial data, safeguarding your equipment, your load, and your operator.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Heavy machineryThink about the heaviest challenges in the open mining, road building and construction industry. Tasks such as cutting through rock or the Arctic permafrost; compacting thick layers of hot asphalt. As well as lifting huge, prefabricated wall panels into place.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Road buildingAdvanced hydraulic systems from Danfoss deliver the machine performance that ensures road builders can meet their deadlines.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Wheel loadersWork with us on new power solutions and experience wheel loader design in a new uplifted way.
Related solutions
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }All-wheel steeringAll-wheel steering is one example of how Danfoss is at the forefront of machine versatility. This helps customers getting the most out of their equipment. Electrohydraulic steering system enables operators to manually adjust the steering mode, allowing them to best match machine performance to the task at hand.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }SteeringAs the global market leader in steering components and systems, Danfoss equips everything from small lawn machines to the largest dump trucks.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Total machine managementOur PLUS+1® platform delivers the software application development power you need — and doesn’t require specialized programming skills.
Case stories
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Volvo excellence awardDanfoss Power Solution India has been honored by Volvo India with the company’s “Project Development Excellence Award”.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }China: No. 1 hydraulic supplier of 2016China Construction Machinery (CCM) rates Danfoss as the No. 1 hydraulic supplier of 2016. The rank is listed in CCM’s annual “Top Suppliers of Construction Machinery in China” list in the October issue of CCM Magazine.
Contact us
For further information, please contact us.