Low(ering) GWP

Seen from a global perspective, the tendency of the industry is to move increasingly toward natural refrigerant solutions when it is technologically safe & economically feasible. Synthetic refrigerants are still likely to play an important role in both the refrigeration and air conditioning industries, where the trend is also moving toward new low-GWP substances that cause a minimal environmental impact.

Read more Read less

Refrigerants having a modest GWP can be sufficient for bringing down emissions. According to the IPCC 5th report, R32 has a GWP of 677 and is a valid substitute for R410A with a GWP of about 1900 thus lowering the impact by 1/3 or even more as the volumetric efficiency is higher than R410A. Another example is the substitution of R404A with R407A or R407F. Here a 50% reduction in GWP is achieved basically at the same efficiency.

These alternatives are lowering the emission considerably while at the same time offering a pragmatic solution, maybe not for ever but at least as a temporary solution.

GWP comparison of refrigerants

Get an overview of the refrigerants options, now and in the future

A paper on the global trends within refrigeration and air conditioning guiding you through today’s and tomorrow’s refrigerants and technologies, with emphasis on global warming potential, energy consumption, system efficiency and other information that will help you stay on top of the game.