Extend the lifetime of your pump systems
Cavitation is a common issue that can have a detrimental impact on the efficiency and reliability of pumps. However, Danfoss variable frequency drives (VFDs) feature integrated condition-based monitoring (CBM) provides new avenues for detecting and avoiding cavitation in pump systems. By utilizing the "VFD as a sensor" approach and current signature analysis, condition monitoring can effectively identify cavitation-related faults and help prevent potential damage and wear-out.
Contact our experts
Like other CBM functions, such as stator winding fault detection, cavitation detection is now considered part of the CBM family. This means that the same CBM infrastructure can be utilized to implement cavitation detection systems. Even (VFDs) with older CBM licenses can be upgraded to feature cavitation monitoring through a software upgrade.
What causes pump cavitation?
So, how does cavitation occur and what makes it a concern for pump systems?
Cavitation happens when rapid pressure changes in a liquid medium cause vapor-filled bubbles to form. These bubbles can collapse under higher pressure, generating shockwaves that create micro-pits in the pump impeller. This leads to accelerated wear-out and erosion of the rotating blades. Additionally, the collapse of bubbles generates additional noise, knocking, and vibration, which further reduces pump efficiency by distorting the flow pattern.
The local implosions of cavitation bubbles can also alter the chemical properties of the liquid, producing free radicals, causing oxidation, and degrading chemical compounds. Although these effects occur in small amounts, they still result in changes to product quality—an important factor in the food and beverage or oil and gas industries.
It is important to note that cavitation can also impact other system components in contact with high-velocity moving fluids, including piping systems, pump components, engine housing, cylinder sleeves, HEX components, and hydro turbine components. So, early detection of cavitation in the pump along with fast remedial action can protect and extend lifespan of a whole system of components.
How does condition monitoring protect pumps against cavitation?
Detecting and avoiding cavitation is crucial for maintaining pump performance and preventing costly damage. Condition monitoring in the form of integrated CBM in the VFD offers an effective solution for achieving this. Cavitation detection can be achieved using current signature analysis in the VFD, enabling sensor-less detection. Cavitation produces turbulence, creating audible noise and a distinctive signature in the motor current. This turbulence is reflected in the motor current and become detected by the condition monitoring algorithm.
The algorithm compares the actual cavitation signature against user-defined threshold levels. If the values exceed the set thresholds for a predefined time, the event is flagged as cavitation.
Benefits of condition monitoring and predictive maintenance
The benefits of avoiding cavitation using condition monitoring are significant. With permanent monitoring using CBM integrated in the Danfoss VFD, both the detection and avoidance of cavitation become possible. This is a cost-effective solution that competes with traditional methods based on external sensors, such as sound, vibration, or pressure. By preventing pump wear-out and damage caused by cavitation, productivity is optimized, and component lifetimes can be extended. It becomes possible to perform predictive maintenance and this ultimately leads to a reduction in service and replacement costs.
Cavitation is one of the killers of pump performance. With condition-based monitoring integrated directly in the VFD, we’re giving our customers a proactive way to detect and prevent damage before it happens. It’s smarter, simpler, and far more cost-effective than relying on traditional sensor-based methods.

Avoiding pump cavitation using condition-based monitoring functionality
To avoid cavitation, the flow can be reduced by lowering the pump speed in small increments. Condition monitoring enables this through an avoidance function. The motor speed is automatically lowered within predefined limits when cavitation is detected. Once cavitation is avoided, the function can be configured either to remain at the last speed that prevented cavitation, or to gradually attempt returning to the original speed reference—continuously checking whether cavitation has disappeared in the meantime. Additionally, the function provides all necessary status information, allowing the VFD to operate as a standalone unit or to be integrated with PLCs into a higher-level process control system. This avoidance function is turned off by default, and it is up to the user to decide whether to activate it based on their specific needs.
In summary, preventing pump cavitation is crucial for maintaining pump efficiency and reducing potential damage and wear-out. Condition monitoring, using advanced techniques such as current signature analysis, provides a reliable and cost-effective solution for detecting and avoiding cavitation. By implementing condition monitoring systems, industrial processes can benefit from improved production, extended component lifetimes, and reduced maintenance costs, ultimately leading to smoother and more reliable operations.
With the edge computing solution, which enables faster insights by processing data at the VFD, data is collected several times per second—ensuring that any measurements outside the normal range trigger a warning quickly and in a timely manner, thus minimizing the risk of undetected abnormalities.

FAQs about pump cavitation monitoring
What is pump cavitation and why is it harmful?
Pump cavitation occurs when rapid pressure drops inside a pump cause vapor bubbles to form and collapse violently. This leads to micro-pitting, noise, vibration, and accelerated wear on impellers and other components. Left unchecked, cavitation can reduce efficiency, damage equipment, and shorten system lifetime.
How does condition-based monitoring detect cavitation?
Danfoss drives use current signature analysis to detect cavitation. When cavitation causes turbulence in the pump, it creates a unique fluctuation pattern in the motor current. The drive analyzes this signal and compares it against baseline values. If the deviation exceeds user-defined thresholds, the drive flags a cavitation event—no external sensors required.
What makes this different from traditional cavitation detection methods?
Traditional methods rely on external sensors like microphones, accelerometers, or pressure transducers. In contrast, the Danfoss CBM solution is fully integrated in the VFD and uses internal data processing. It’s more cost-effective, easier to maintain, and enables continuous monitoring without extra hardware.
What happens when cavitation is detected?
The integrated avoidance function automatically lowers the pump speed within preset limits to eliminate cavitation. Once resolved, the VFD can maintain the new speed or attempt to return to the original speed reference—continuously monitoring whether cavitation returns.
How does this improve pump system reliability?
By catching cavitation early and automatically adjusting operation, condition-based monitoring helps prevent damage, reduce maintenance costs, and extend pump and system lifespan. It supports predictive maintenance strategies and helps improve process uptime.
Which applications benefit most from cavitation monitoring?
Industries with critical pump systems—such as water and wastewater, food and beverage, oil and gas, and chemical processing—gain the most value. Cavitation detection is especially useful in remote or difficult-to-access locations, where traditional inspections may be delayed or impractical.
Contact our experts
Are you experiencing issues with pump cavitation? Our expert, Tim Flintholm Fink, is ready to assist you and discuss solutions.
Submit your queries below to get in touch with Tim for an informal discussion.

Drives for pump applications

By controlling industrial pumps with a Danfoss AC drive you can help optimize processes and significantly reduce energy and maintenance costs.

For reliable operation, reduced emissions, and long life of marine pumps and separators, draw upon engineering knowhow from Danfoss.

Enhance your system performance, extend your equipment life, and protect against leakages, by optimizing pump operations using Danfoss AC drives.

Protect your pump and optimize commercial ventilation and air conditioning performance using AC drives.
Explore more opportunities with CBM

VFDs act as intelligent sensors for condition monitoring in automated systems. Explore features of intelligent drives and various maintenance strategies.

Monitoring motor performance using condition-based monitoring provides a simple and cost-effective way to obtain machine data for smart maintenance decisions.

Predictive maintenance has emerged as a powerful tool to optimize equipment performance, increase uptime, and reduce maintenance costs.

Along with stator winding monitoring and load envelope, the CBM functionality integrated into Danfoss drives includes vibration monitoring.

Remote monitoring empowers users to access real-time data, react early to avoid interruptions, optimize performance, and make informed decisions.

Refrigeration systems preserve apple quality using VSDs with integrated condition monitoring and DrivePro Remote Monitoring service
ITALY: At Rivoira Group, VLT® drives with built-in condition-based monitoring help preserve fruit perfectly by ensuring utterly reliable refrigeration.
Read the case study

Driving maximum uptime in aseptic pharmaceutical production
DENMARK: A leading global pharmaceutical company was determined to find an intelligent HVAC solution to prevent downtime with real-time system monitoring and customizable instant alarms. Plus, the solution needed to fit within the organization’s ambitious digitalization strategy. The solution: Danfoss VLT® HVAC Drive FC 102 with integrated condition-based monitoring.
Read the case study

Brewing up real change at HEINEKEN
NETHERLANDS: HEINEKEN understands that to meet demand, its production line must always be up to the task – with all assets expected to deliver a consistently reliable and excellent performance. At Den Bosch brewery, the tough working environment posed several challenges. The solution was an upgrade using drives with integrated condition-based monitoring.
Read the case study