• My Apps
    My Apps You will have the option to use My apps once you login.

Retrofitting Keppel Bay Tower for a Zero Energy future

Tuesday, January 24, 2023

SINGAPORE: A landmark in Singapore’s Keppel Bay waterfront area, the 18-story Keppel Bay Tower is a true testament to Keppel's commitment to sustainability and unrivaled energy efficiency.

Following a retrofit project implementing the Danfoss EC+ concept for optimal system efficiency — featuring Danfoss AC drives, NOVENCO axial fans, and high efficiency motors — Keppel Bay Tower achieved energy savings of more than 45% in AHU operation, which contributed to making it Singapore’s first BCA Green Mark Platinum Zero Energy commercial building.

Keppel Bay Tower

>45% energy savings with EC+ concept

What's the influence of efficiency in buildings like Keppel Bay Tower? Good building management saves more energy than you might think.

3 men installing a ZerAx fan, and the text "Less than 10 hours for retrofit work"

The challenge: Reduce energy consumption by at least 20%

In 2018, Keppel Land leveraged a grant from the Building and Construction Authority of Singapore Government (BCA) under the Green Buildings Innovation Cluster (GBIC) Programme to implement and test new energy efficient technologies at Keppel Bay Tower to reduce the building’s energy consumption. The tower had already achieved the BCA Green Mark Platinum status but the aim of the GBIC initiative was to reduce energy consumption by a further 20%.

Danfoss, along with long-term partner NOVENCO, proposed retrofitting an existing centrifugal fan in one of the building’s air handling units (AHU) with the high efficiency EC+ concept engineered to boost the efficiency of HVAC systems in both new-build AHUs and in existing systems.

The Danfoss-NOVENCO EC+ concept proposal, which leverages the high efficiencies and integration ease of VLT® HVAC Drive FC 102, motor, and ZerAx® fans, was reviewed by industry experts appointed by the BCA and independent researchers. They could clearly see energy reduction potential in the EC+ concept combining some of the most innovative technologies in the market — while offering an easy retrofit to minimize downtime and inconvenience.

Man programming a HVAC FC 102 drive

The solution: Quick retrofit with EC+ concept

As one of five technologies chosen for the GBIC initiative, the EC+ concept enables significant reduction of energy use in AHUs by means of three components: intelligent Danfoss VLT® drives, NOVENCO’s highly efficient ZerAx® axial flow fans, and IE4 and IE5 permanent magnet (PM) motors.

The concept is characterized by two key factors — namely the high efficiency of each of the individual components as well as their intelligent interaction. The result is a seamless, fully compatible solution that enables realization of its full potential delivering optimum system efficiency. Also, the EC+ concept offers a low-risk solution by utilizing only time-tested, proven technologies.

Unlike the centrifugal fan, axial fans utilize both the static and the dynamic pressures. The ZerAx® fan is therefore more efficient, consumes less energy, reduces operating costs, and lowers carbon emissions — plus, it reduced the sound level significantly.

Variable speed drives enable energy efficient application control, which makes them key to achieving energy savings in building operations. A HVAC-dedicated drive with built-in intelligence, the Danfoss VLT® HVAC Drive FC 102 is known for its high reliability, low total cost of ownership (TCO), and many application functions. This made it the perfect match for Keppel Bay Tower as a modern building fitted with a wealth of sophisticated solutions.

The retrofit — done in January 2019 — was completed in less than 10 hours.

Outside of Keppel Bay Tower, with the text "22.3% reduction in annual energy consumption"

The outcome: Green Mark Platinum Energy Zero building

The EC+ AHU retrofit delivered energy savings of more than 45% for Keppel Bay Tower — as well as a more pleasant environment for the building occupants thanks to the lower sound level. This result played a significant part in the 22.3% reduction in the building’s annual energy consumption as of February 2020 — exceeding its initial target of 20%.

Recognizing the company’s efforts, Keppel Bay Tower was therefore certified by the BCA as a Green Mark Platinum Zero Energy building — the first commercial building of its kind in Singapore. And its new high efficiency air distribution system based on the EC+ concept was one of the key contributors to this achievement.

Read the case story as PDF

Get even more drive in your HVAC

Get even more drive in your HVAC

Read more about Danfoss HVAC solutions

More AHU case studies

  • if (isSmallPicture) { The Loves-Park-Factory-Building; } else if (isBigColumns) { The Loves-Park-Factory-Building } else { The Loves-Park-Factory-Building }
    Ventilation is more energy-efficient in this Illinois factory

    USA: The Danfoss Loves Park factory upgraded existing ventilation with the Danfoss Novenco EC+ concept, achieving a 59.8% reduction in emissions compared to the previous system.

  • if (isSmallPicture) { Man flying in the wind tunnel; } else if (isBigColumns) { Man flying in the wind tunnel } else { Man flying in the wind tunnel }
    Wind tunnel achieves 99.5% uptime with Danfoss DrivePro®

    Belgium: Thanks to Danfoss DrivePro® services, LuxFly has achieved 99,5% uptime in Europe’s largest vertical wind tunnel that is used for skydiving.

  • if (isSmallPicture) { The factory seen from afar with a sunrise in the back ; } else if (isBigColumns) { The factory seen from afar with a sunrise in the back } else { The factory seen from afar with a sunrise in the back }
    How did this smart factory reach carbon-neutral?

    POLAND: The new Danfoss production hall in Grodzisk Mazowiecki has reached carbon-neutrality, thanks to full electrification, energy-saving solutions such as Danfoss drives, and energy from renewable sources.

  • if (isSmallPicture) { Keppel Bay Tower sign with the text "More than 45% energy savings with Danfoss-NOVENCO EC+ concept"; } else if (isBigColumns) { Keppel Bay Tower sign with the text "More than 45% energy savings with Danfoss-NOVENCO EC+ concept" } else { Keppel Bay Tower sign with the text "More than 45% energy savings with Danfoss-NOVENCO EC+ concept" }
    Retrofitting Keppel Bay Tower for a Zero Energy future

    SINGAPORE: With Danfoss EC+ concept for HVAC systems, Keppel Bay Tower uses 45% less energy and has achieved Green Mark Platinum Zero Energy building status.

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Drives secure fresh air inside South America’s tallest building

    A huge number of Danfoss drives secure comfortable temperatures and cut down energy use inside Chile’s famous Costanera Center.

  • if (isSmallPicture) { Driving maximum uptime in aseptic pharmaceutical production; } else if (isBigColumns) { Driving maximum uptime in aseptic pharmaceutical production } else { Driving maximum uptime in aseptic pharmaceutical production }
    Driving maximum uptime in aseptic pharmaceutical production

    DENMARK: A leading global pharmaceutical company was determined to find an intelligent HVAC solution to prevent downtime with real-time system monitoring and customizable instant alarms. Plus, the solution needed to fit within the organization’s ambitious digitalization strategy. The solution: Danfoss VLT® HVAC Drive FC 102 with integrated condition-based monitoring.