Balancing energy in municipal and industrial wastewater treatment
Since water and wastewater treatment processes account for 4% of global electricity consumption, it's vital that reducing energy consumption is in focus for industrial and domestic wastewater treatment. Not only for sustainability but also for economic reasons.
Transformation of municipal wastewater treatment plants from energy consumers into energy generators now couples the water and energy sectors together into a new game-changing industry. Regulation of rotating equipment is a vital element in generating over 100% surplus power in wastewater treatment, for energy-neutral water cycle management of entire communities.
Discover how drives can revolutionize the water sector, in our whitepaper: The potential of the water-energy nexus.
Substantial amounts of fresh water are consumed in modern society and all too often poorly treated wastewater is discharged into the environment. To counter these trends, modern digitalization offers a great degree of controllability in municipal wastewater treatment resulting in higher quality of treated water. And ZLD and MLD processes reduce the volume of industrial wastewater discharge.
To improve the reuse of water and reduce the discharge of industrial wastewater, a zero liquid discharge (ZLD) or a minimal liquid discharge (MLD) treatment system is often used. ZLD and MLD are ambitious wastewater management strategies that enable the plant or facility to recover most of its wastewater for reuse. The standard process is energy intensive, but applying optimized reverse osmosis processes energy consumption can be reduced by up to 75%.
Wastewater treatment plants
Typically, water and wastewater treatment processes account for 25-40% of a municipal electricity budget. Water and wastewater facilities are therefore normally the single-largest electricity consumer for a municipality. Therefore for many years, extensive use of AC drives and real-time online sensors have created the basis for advanced real-time process control to optimize energy efficiency, cutting energy consumption by 20–40%.
Now these methods combine with energy production within the wastewater treatment plant, to enable entirely new ambitious levels of energy efficiency. Powered by methane produced in the digester of the wastewater plant, the 'bio refinery' or 'Water Resource Recovery Facilities' demonstrate that wastewater has now become an energy resource.
Some of the most advanced water management systems achieve complete energy self-sufficiency of the water cycle. The energy recovered from wastewater treatment process not only covers the plant's own needs, but also the energy needs for drinking water production and distribution as well as wastewater pumping. In other words, the whole water cycle can be considered energy neutral.
A precondition for energy neutrality is a control handle in the form of an AC drive available for all rotating equipment, so that the fully computer-controlled facility can adapt to the changing load.

Generating surplus power from wastewater treatment
Cities could eliminate 300 Mill t CO2e emission by applying the best available wastewater treatment techniques globally.
Read the whitepaper
Tackling water scarcity with efficient ZLD and MLD water treatment
To improve the reuse of water and reduce the discharge of industrial wastewater, Zero Liquid Discharge (ZLD) and Minimal Liquid Discharge (MLD) have emerged as highly efficient wastewater treatment processes.
ZLD and MLD are ambitious wastewater management strategies, which eliminate/reduce any liquid waste leaving the plant or facility with most water being recovered for reuse.
The efficient reduction of effluent makes the ZLD and MLD processes highly attractive to industries and utilities. Until now, however, the processes have been constrained by high costs and intensive energy consumption. The traditional thermal-based process used in ZLD/MLD systems is highly energy intensive. By adding a membrane-based process, studies show that energy consumption can be reduced by up to 75%.
Learn more about how to use our APP W HC pumps in ZLD reverse osmosis applications
Read the complete case story here

Stormwater overflow
Optimization of the wastewater canalization system using pump regulation can improve pump efficiency by 15–30% and also drastically reduce maintenance costs in managing stormwater overflow.
The traditional solution for combined sewer systems to limit storm water overflow, is to build major storage tanks on the sewer network, which then can store the high volume of water arising with heavy rain.
Using digitization, and connected to a high-granularity weather radar system, highly accurate rainfall analysis can be integrated. By managing capacity optimally, the utility can reduce capital investment. Digitization also enables them to operate a warning system, in the rare event that a sewer overflow does occur.

Reduce the risk of unexpected downtime
Did you know your Danfoss drive can monitor system health to deliver early warnings of wear or malfunction? Activate integrated intelligence on the edge to enable condition-based monitoring (CBM) for high uptime and optimal maintenance planning.
Discover CBM
Related products

The Danfoss iC7-Aqua is the next-generation variable frequency drive for pumps, meticulously designed for water supply, wastewater, desalination, irrigation, and industrial pumping applications. It’s built on a new, modular platform that ensures robust performance, advanced process control, and a future-proof design to meet the evolving demands of the water industry.

VLT® AQUA Drive FC 202 controls all types of pumps and comes equipped with a cascade controller.

With a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, active iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day

The APP W HC pump is suitable for ZLD and MLD reverse osmosis applications used in industrial wastewater treatment.

At Danfoss, we have always been dedicated to maintaining the longevity and performance of your equipment through our out-of-warranty repair services. Our new Fixed-Price Repair Program builds on this commitment by offering not only repairs but also upgrades to older products with the latest parts. This ensures optimal performance and reliability, allowing you to extend the life of your equipment.
Related applications

Use AC drives to control the speed of motors in a wide range of pump, blower, mixer and dewatering applications to help enhance performance and value while saving energy and costs in wastewater treatment.
Learning
Save energy with a membrane-based process
Most ZLD/MLD systems are operated with a thermal-based process as standard. This process puts a great demand on energy consumption, making it a very expensive investment.
One way of reducing energy consumption is to reduce the amount of water that needs to be evaporated by changing from a thermal to a membrane-based process. This is supported by studies that show an efficiency gain of up to 75% when going from the thermal-based to the membrane-based process.
How business benefit from applying a ZLD or MLD treatment system
Zero or minimal liquid discharge are some of the good answers to the global water crisis. Both technologies help to meet discharge and water reuse requirements enabling businesses to meet regulations, protect the environment and improve management of the water produced.

ZLD and MLD make industrial wastewater clean again, ready to reuse. It relieves the pressure on freshwater reserves and helps to protect the environment.

ZLD and MLD systems help to meet the strict environmental regulations for wastewater treatment introduced in many regions of the world.

Among a wide range of technologies, industries and utilities prefer ZLD/MLD as best in class solutions due to its efficiency and low operating costs.

Rethinking the water sector
Energy generation and water management are intricately entwined. Today, technologies designed to create an energy-neutral water sector are already available.
Discover more
Support videos
Case stories

VLT® AQUA drives recently installed at the Chertsey Water Treatment works of Affinity Water deliver savings of more than a third of a million pounds in running costs.

Wastewater treatment plant’s use of AC drives on rotating equipment creates net production of both electricity and heat and reduces its carbon footprint by 35%.

China's zero liquid discharge legislation (ZLD) is driving increased use of RO technology to treat industrial wastewater. Danfoss APP pumps are increasingly in demand to make such ZLD projects as energy-efficient - and profitable - as possible.

To reduce the significant energy costs that result from wastewater being transformed from liquid to solids, companies are turning to RO treatment – and Danfoss APP pumps are helping to keep energy costs at a minimum due to high efficiency.