Strong performance
Ships of all sizes need a skillful captain to maneuver them into port, where space is often tight and the weather can be unpredictable. They rely on thrusters on the vessel sides to help them. For strong thruster performance, Danfoss has developed a range of propel systems and intelligent controls. Today, fast and efficient docking is a much easier job.
With a turning capability of 360°, thrusters can push a ship in any direction. Maneuverability is particularly powerful when multiple thrusters are installed.
Using our advanced electrohydraulic components and controls, it’s possible to enhance thruster performance with variable propel speed and even variable blade control. The proportional PVG valves and H1 hydrostatics deliver thruster power in an integrated system that can be linked by CAN bus with other control systems on board. That’s a big advantage – particularly when hydraulic components are located in different parts of the ship.
Documents
| Type | Name | Language | Valid for | Updated | Download | File type |
|---|---|---|---|---|---|---|
| Brochure | Marine, Oil and Gas Certification Brochure | English | Multiple | 03 Nov, 2019 | 541.0 KB |
Related products

Application specific track and swing drive motors.With industry leading geroler® design, these orbital motors secures excellent efficiency, two speed and low slip performance designed for mini-excavators

Thanks to the easy-to-fit design the CLM T cam lobe motor is a perfect fit for compact track loaders, and other tracked construction machines.
Related applications
Related solutions
Case stories

Danfoss Editron and Spierings Mobile Cranes work together to develop mobile cranes and lifts that generate zero emissions. As of 2020, all the machines manufactured by Spierings have electric functionality. This use case explores the partnership.

Molslinjen – Denmark's largest domestic ferry company – has set its first electric ferry in motion. The E-ferry Grotte will be breaking waves at the UNESCO World Heritage waters between the coastal town of Esbjerg and the island Fanø – and Danfoss is on board. The future holds great potential to operate shorter routes by electric ferries.

European manufacturer Kovaco has a strong track record of developing products that push the limits of technology, efficiency and environmental performance. The company’s Kovaco Electric division provides sustainable solutions for the future, offering environmentally-friendly and cost-efficient products with high safety levels.

The mining industry is increasingly turning to commercial vehicle electrification solutions for the machinery used during operations because of the performance and safety benefits they offer

E-ferry Ellen is an excellent example of the future for electric transport: cleaner, greener and more efficient. A great Danfoss Editron project which demonstrates the potential for electric ferries to end users and the industry itself.

For retrofitting the iconic Finnish ferry - Prostvik, Danfoss Editron introduced its new direct current-link solution, consisting of a compact and lightweight diesel-electrical drivetrain. The main benefits of installing a diesel-electric system are significantly reducing the ferry’s environmental footprint, as well as achieving redundancy.
Contact us
For further information, please contact us.