• My Apps
    My Apps You will have the option to use My apps once you login.

Meeting Growing Market Needs: Danfoss Extends DMB/DCB Bi-Flow Filter Drier Production to India

Thursday, October 12, 2023

Danfoss has inaugurated a new production line in India dedicated to the manufacturing of DMB/DCB bi-flow filter driers, in response to the escalating demand within the market. The newly designed bi-flow filter driers showcase subtle re-engineering, resulting in heightened system performance:

  • They boast an elevated maximum working pressure and temperature, reaching 50 bar* and 120°C respectively.
  • 20% more moisture capacity versus NBA
  • These filter driers are fully compatible with main A2L and A3 refrigerants needed in new platforms.

*From India factory

The expansion of production operations in India, coupled with continuous support from the production team in Mexico, enables Danfoss to accomplish global distribution of filter driers in remarkably swift timeframes. This translates to sustained availability and expedited delivery for customers worldwide.

The filter drier constitutes a pivotal component in ensuring the system's reliability and lifespan. Danfoss offers an extensive selection of filter driers encompassing both hermetic and exchangeable core variations. The core's role is to enhance the filter drier's capacity to adsorb moisture and acids, effectively preventing corrosion of the compressor's metallic surfaces, while simultaneously safeguarding against decomposition of oil and refrigerant.

Learn more about Danfoss' filter driers:

The Filter drier is a vital element of the system’s reliability as well as its lifespan. Danfoss’ range of Filter driers covers both hermetic and exchangeable core types. The core makes the Filter drier absorb water and acids more effectively to prevent corrosion of the compressor’s metal surfaces and ensure that oil and refrigerant do not decompose.

Coolselector®2

The truth is Cool(selector®2)

Coolselector®2 features unbiased calculations for the selection of refrigeration and air conditioning components based on the user’s requirements or based on standard operating conditions.