Royal IHC Scheldt River pioneers new environmental standards in dredging with flexible MV drives

Wednesday, February 12, 2020

NETHERLANDS: The Scheldt River is a 7950 m³ dual-fuel (diesel and LNG) hopper dredger designed and built by Royal IHC in the Netherlands for DEME. It represents the latest in hybrid dredging technology with its “flex fuel” main engine capable of running on natural gas or light fuel oil. The dredger is part of DEME’s innovative Trailing Suction Hopper Dredger fleet.

With its ‘Green Passport’ and a ‘Clean Design’ notation, the vessel complies with the strictest international emission requirements. To help achieve these high standards, Danfoss was asked to contribute a drive solution that could boost an inboard dredge pump and increase energy efficiency with a small footprint, minimum weight and low volume - while being robust enough to withstand the harsh marine environment.

Discover how modular MV drives helped win the 2018 Ship of the Year award

Performance and flexibility

Performance and flexibility

The modular VACON® 3000 Drive Kit qualified for the project for its ability to contribute to the vessel’s overall green performance and to offer the flexibility of design required by IHC’s engineers and technicians. This MV kit package enabled IHC to make their own customized, integrated solution, the IHC MV drive.  Based on a modular approach, the compact IHC MV drive helps to save space and weight, optimizing the overall design of the vessel and its equipment.

A partnership of experts

A partnership of experts

When configuring and installing the VACON® 3000 drive, IHC was able to draw upon the experience of application experts in Danfoss Drives’ Marine Application Development Centre in the Netherlands. The centre is equipped with a range of testing and demo units, which were used to help and facilitate complete panel testing on load and customer FAT, together with IHC.

The keys to energy efficiency

The boosting of the vessel’s dredge pump with an AC drive was made possible through power take-in (PTI) technology, which allowed load sharing between the VACON® 3000 and the main dual-fuel engine. This resulted in significantly higher energy efficiency.

Using transformer-less AFE technology employing normal water-cooling, the VACON® 3000 drive can run on lower supply frequency and voltage.

Efficient dredge pumping

Efficient dredge pumping

VACON® NXP LV drive modules are employed for other applications including pumps, thrusters and active filters. The switching of drive control between the inboard dredge pump and the submersible dredge pump of 1700 kW is performed by a medium voltage switchboard, where also the required sinus filter is located.

Replicating award-winning performance

The Scheldt River has been in operation since 2017, and in 2018, IHC was declared winner of the Maritime Award, ‘KNVTS Ship of the Year’, for taking a major step towards cleaner dredging. To continue setting new standards in environmental performance for the dredging industry, ship owners, DEME, have placed an order with IHC for an additional vessel of the same specifications, the dredger, Meuse River, which utilizes the same VACON® 3000 Drive Kit.

The VACON® 3000 Drive Kit fulfilled IHC’s requirements for suitability for a marine environment, minimum weight, small footprint and low volume. The power module design was especially well-suited to the harsh environment, being equipped with specific measures to avoid dust of any kind and pollution contaminating the semiconductors during ship construction.

Related applications

  • Drives for marine power conversion and generation
    Drives for marine power conversion and generation
    Draw upon expertise from Danfoss to optimize energy storage solutions using drives for power conversion both on board vessels, and in shore power supply for quieter and cleaner harbors.
  • Drives for marine propulsion and thrusters
    For more efficient operation and greater freedom in ship design, consider an electric-based main propulsion with engineering from Danfoss.