Growing potatoes without soil
NorStar Corporation has produced standard aeroponic irrigation systems since 2010. In 2017, the U.S.-based company embarked on the development of its proprietary high-pressure aeroponic, or “fogoponic” irrigation system for commercial use. While the company’s standard aeroponic systems had already produced record yields, its latest fogoponic innovation has increased these by twofold – all while dramatically reducing the propagation cycle, thus revolutionizing how potato seeds are produced. Danfoss PAH pumps provide the reliably clean pressure.
The challenge: Provide high-pressure with the highest possible reliability and purity
NSC’s engineers’ most important demand for the high-pressure pumps for its potato seed production facility in Israel was reliability: Any prolonged failure to keep the growing plants’ roots surrounded by nutrient-rich aerosols would kill off the time-consuming, high-value crop. The complex arrangement of nozzles, sensors, algorithms, and apps would do their part to maintain exact pH and electrical conductivity levels for the nutrients, but the pumps must also do theirs around the clock.
But equally important to NSC was cleanliness. Just as no diseases could be tolerated in the greenhouse environment, contamination of any kind from the facility’s high-pressure pumps was a no-go.
The solution: Reliably clean Danfoss PAH pumps
According to Talal Daas, NSC’s CEO, the search for the right high-pressure pump quickly led to the Danfoss PAH high-pressure positive displacement pumps – the only pumps on the market to meet all of their demands.
“We have previously used Danfoss PAH pumps, so we were familiar with their specifications and benefits,” he says. “For this important pilot installation of our newest production technology, there was no doubt. We needed Danfoss’ unrivaled pump reliability to ensure failsafe operations 24/7. The fact that the pumps use no oil for lubrication sealed the deal – we must be 100% certain that the pumps could never spread any contamination that could put this high-value production at risk.”
The high-pressure aeroponic system that NSC deployed in Israel contains three Danfoss PAH 6.3 pumps. Like all of NSC facilities, redundancy is built into system design. Even though all three pumps are dedicated to specific tasks, each of them can automatically take over the task of any of the two other pumps in the event of failure.
The results: Perfect pump performance does its part to ensure revolutionary growing method
Over the six-month growing cycle necessary to propagate the potato crop, the Danfoss pumps performed flawlessly, and NSC’s prototype facility produced amazing results that far surpassed even their most optimistic hopes.
“On the way to these breakthrough results, we faced a number of other challenges,” recalls Daas, “but the Danfoss pumps were never one of them. Despite constant use for six months, no maintenance was ever needed, and they required no attention at all as they simply did their job. We were surprised by one thing, however – how quiet the installation’s little machine room was. Normally, being so close to high-pressure pumps makes conversation practically impossible, but the Danfoss PAH pumps were far quieter than expected.”
With strong market appeal to potato growers worldwide, NSC has high hopes for the future of their innovative new technology. “We are already in negotiations with a number of international customers,” reveals Daas, “and we are convinced that the Danfoss PAH pumps will be standard in all our coming installations. In addition to being available without much lead time, they are small and light enough to transport easily – and they have already proven their role in our results.”