Even though Canaragua has installed dozens of SWRO plants throughout the Canary Islands, the project in Puerto de Mogán was unusual because of the focus on compactness. The municipality needed to expand water production, and the best place to locate the new plant was in the middle of the historic town right off the main square. Could Canaragua come up with a containerized solution that was compact enough to fit in the small allotted space?
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) {
} else {
}
iSave® energy recovery devices for high-pressure membrane applicationsWith a 3-in-1 design that integrates highly effective isobaric pressure exchangers with positive displacement booster pumps and electrical motors, iSave® ERDs deliver big energy savings in small spaces. Covering train sizes from 200-3,000 m3/day
-
if (isSmallPicture) {
; } else if (isBigColumns) {
} else {
}
High-pressure pumps for SWRO applicationsThe range of high-pressure APP pumps is optimized for both landbased, off-shore and marine sea water reverse osmosis applications. Available with or without motor.