• My Apps
    My Apps You will have the option to use My apps once you login.

Data center power consumption

Data center power consumption

The demand for internet and smart technologies makes it vital that we reduce electricity use in data centers and implement more efficient energy solutions to create data center sustainability and cut CO2 emissions.

Inside data center

Data center sustainability – a more efficient future is needed

By 2025, every person in the developed world will have at least one ‘interaction’ with a data center every 18 seconds of their lifetime. Our demand for internet and smart technologies is increasing rapidly.

The numbers above highlight what is happening online in just 60 seconds, showing that in the near future our demand for internet services will be huge. At the same time, power usage within the information industry is growing rapidly. This makes it vital that we reduce electricity use in data centers and implement more efficient energy solutions to create data center sustainability and cut CO2 emissions.

Data center at the Danfoss headquarters in Nordborg

So, what is a data center?

All data centers are simply buildings that provide space, power and cooling for network infrastructure and are filled with varying amounts of servers. Data center power consumption is directly related to the number of servers they have. Data centers store, share, and manage data and centralize key IT operations and equipment. They can be categorized by business model, ownership structure and location.

Of the five main types of data center, edge data centers – a data center that is strategically located in an area near where the data is being collected and analyzed – are expected to have the most significant growth in the data center market and is expected to nearly triple by 2024. By 2025, more than 75% of enterprise-generated data will be created and processed outside the traditional data center or cloud.

How is data center power consumption efficiency measured?

Data center power consumption performance is measured in units of Power Usage Effectiveness (PUE).  PUE is a limited-focus design, real-time and annual measurement of the total facility power divided by the IT equipment power, or a measurement of energy ‘waste’ going to non-IT equipment purposes.

An ideal PUE is 1.0, that means 100% efficiency (i.e., all consumed energy is used only on IT equipment, no power distribution loses). But it is almost impossible to achieve. The average power usage effectiveness (PUE) ratio for a data center in 2020 was 1.58, only marginally better than 7 years ago, according to the latest annual Uptime Institute survey.

In addition to PUE, alternative metrics that account for waste heat utilization have been suggested, for example PUErecycled and ERE (energy reuse effectiveness). These units indicate the net energy consumption of the data center after factoring in reused energy.

Data center, close up from a server room

What is the challenge for data centers?

The majority of the energy demand in data centers comes from powering the servers, but they in turn produce heat and need to be cooled. This cooling again requires a lot of energy and generates a lot of excess heat – most of which is currently being let out into the surrounding environment.

To reduce data centers’ carbon footprint, a smart combination of innovation and technology is needed to reach net zero emissions. Fortunately, there are already more energy efficient solutions available to make the most of the energy we put into our data centers.

How can policies make data centers greener?

There are several steps policy makers can take to help implement green solutions for data centers. For example, they could:

  • Design a regulatory framework which encourages systems integration and the use of waste heat, heat pumps, smart heating and cooling systems, and energy storage. It should focus not only on greening energy sources but encourage reduced use and reuse of energy.
  • Improve energy planning to better integrate the different sectors to the energy system and leverage synergies, such as utilizing the waste heat from a nearby data center to heat buildings instead of investing in additional heat supply.
  • Allow urban regulatory free test zones to innovate and develop new energy efficient technology, through removing technical, regulatory and financial barriers for reusing energy between sectors.
  • Encourage thermal networks by introducing a facilitating framework. Elements include allowing flexible energy prices and not taxing waste heat.

How can Danfoss help decrease power consumption of data centers and increase their energy efficiency?

There are many ways in which it is possible to create greener data centers and to process data sustainably. Danfoss solutions help the full range of data centers reach high power usage effectiveness (PUE) and energy reuse factor, while supporting reliably high uptime. From data center cooling sources such as chillers, to piping distribution network, to cooling terminals, close control units, air-handling units (AHUs), fans and pumps, and electric heating to protect pipes, we offer a wide range of innovative solutions to deliver highly reliable cooling and reduce energy cost in a sustainable way.  

Data center cooling

What is the most efficient way to cool data centers?

IT cooling is vital because it protects equipment. By optimizing the capacity of IT equipment and preventing expensive downtime, Danfoss solutions create ideal thermal conditions around server installations, while optimizing PUE, keeping energy consumption and CO2 emissions at a minimum to generate more data more sustainably.

Find solutions for cooling data centers

Heat recovery and sector coupling

How Danfoss utilizes sector integration for greener data centers

By using district heating and solutions for heat pumps, Danfoss provides reliable and innovative solutions for data center heat recovery and sector integration, which eventually leads to carbon neutrality and greener data centers.

Find solutions for heat recovery and sector coupling

Danfoss headquarters, Nordborg, Denmark

How does energy storage contribute to sustainable data generation?

Integrated energy storage ensures a reliable supply to the data center, overcoming an unreliable grid or the intermittent nature of many renewable energy sources. Danfoss solutions ensure reliable power conversion for energy storage in smart distribution grids and enable peak shaving. This is where energy storage smooths the peaks and troughs, so the grid supply can operate consistently at the average power demand - which is usually relatively low.


Find solutions for energy storage

Find more data center stories

Data center power consumption FAQ

By using the most efficient technologies to protect and cool the IT equipment.

Through sector integration, the excess heat produced by data centers can be used in district heating networks to heat the nearby communities. Besides using renewable energy, data centers can significantly reduce the amount of energy they use by installing the most efficient cooling systems. Furthermore, the excess heat produced can be reused to help decarbonize district heating networks.

A green data center uses the most efficient technology for protecting and cooling the IT equipment in order to use as little energy as possible. It reuses excess heat to make the most of the energy and uses renewable energy to further avoid CO2 emissions.

The most efficient way to cool data centers depends on the site size, location, and architecture. Danfoss offers a wide range of innovative solutions such as chillers, piping distribution network, cooling terminals, close control units, air-handling units, fans and pumps, and electric heating to protect pipes.

Find energy efficient solutions for data centers at datacenters.danfoss.com

Explore related articles