The event takes place 5 to 8 November in Amsterdam, the Netherlands. Danfoss will be present in hall 12, booth 12.703.
In recent years, the number of desalination plants has increased along the coastlines of many continents. And the number is likely to continue to grow in the coming years as a natural response to the increasing water scarcity facing the world today.
The global water challenges call for innovative solutions and Danfoss is committed to supporting with expertise and unique technologies that can make SWRO solutions even more efficient without compromising the environment.
At Aquatech Amsterdam 2019, Danfoss exhibits core technologies for efficient desalination: The APP high-pressure pumps, the iSave Energy Recovery Devices and the new DST P40I pressure transmitter.
“Our target is to develop, manufacture and market innovative solutions for the demanding reverse osmosis (RO) market. We constantly work with our customers to make sure we meet the needs in the market”, says Jesper Bentzen Sales Director for Danfoss High Pressure Pumps.
Core technologies for various SWRO applications
High-pressure pumps, energy recovery devices, AC drives and pressure transmitters from Danfoss combine into sustainable and highly efficient desalination solutions that return substantial energy savings in both small containerized units up to larger trains of parallel-coupled pumps and ERDs.
“At Aquatech Amsterdam 2019, we will not only exhibit our APP pumps and iSave ERDs. We will introduce our core technologies from Danfoss, and be ready to explain how you with the whole package can save up to 65% on energy costs”, Jesper Bentzen ends.
At the Danfoss booth, which this year is located in hall 12, you can explore the range of APP pumps used in more than 20,000 SWRO plants around the world to obtain maximum efficiency, reliability and flexibility in system set-up. You can learn more about the patented iSave ERD, scalable for use in SWRO applications of any size and type. You can also experience the new Danfoss DST P40I titanium pressure transmitter, designed to meet requirements in corrosive environments as desalination systems.
Additionally, you can learn about the APP W HC pump recently released for ZLD/MLD industrial waste water treatment, built for outlet pressures of up to 120 bar and reducing energy consumption of ZLD/MLD plants significantly.
You will find us at booth 12.703, hall 12, RAI Amsterdam, the Netherlands.
More information about Aquatech Amsterdam
About Danfoss
Danfoss High Pressure Pumps, member of the Danfoss Group, develops and manufactures axial piston pumps and isobaric energy recovery devices for demanding applications in a broad range of industries such as reverse osmosis. Danfoss Drives and Danfoss Industrial Automation, also members of the Danfoss Group, develop drives and pressure transmitters which among other things are suitable for demanding applications such as seawater RO. With tomorrow’s challenges within water scarcity, Danfoss is committed to innovation and has an eye on the future, Danfoss is engineering tomorrow.