Basic component selection
Here, we will go through creating a project in which we try selection and calculation for a few components in a very simplified refrigeration cycle as it can be seen in the following graph and properties snippet. We will also discuss how to customize the project with your own name, how to get bill of materials and how to generate a report for this project. Make sure your preferences choice is set to “’all applications’ in “Options | Preferences | All applications”:
System properties 1
Cycle diagram 1
For the following explanations on basic component selection, we will use the information in System Properties 1 and Cycle Diagram 1 above.
First, and to give you an overview of the “Valves and Line Components” part of Coolselector®2, we will start by selecting a DCA-DA burnout filter for the suction line in a dry system with the default operating conditions.
To do this, open Coolselector®2. Upon doing so, you will find that the program starts on the tab for ‘Valves and Line Components’. From this screen, among the different component functionalities, we will choose “Burnout filters”.
Coolselector®2 creates a dry system by default, and we then select the suction line and then click on the DCR-DA in the product families. You will see the list of valid products and the best one matching the selection criteria as depicted in the snippet below:
Here you can also see the other parameters for the filter in the table, such as acid capacity, as well as the pressure-drop as a function of changing the cooling capacity and keeping the other parameters constant.
Contact us
For further information, please contact us.
News
Documents
Type | Name | Language | Valid for | Updated | Download | File type |
---|---|---|---|---|---|---|
Promotion material | Coolselector®2 Exercises | English | Multiple | 04 Jun, 2019 | 13.5 MB | |
Installation guide | Coolselector®2 Server Installation Guide | English | Multiple | 18 Nov, 2020 | 1.2 MB | |
User guide | Coolselector®2 User Guide | English | Multiple | 04 Jun, 2019 | 4.4 MB | |
User guide | Coolselector®2 User Guide | Spanish, Castilian | Spain | 25 Feb, 2020 | 5.8 MB | |
User guide | Coolselector®2 User Guide | Portuguese | Multiple | 03 Jan, 2020 | 5.3 MB | |
User guide | Coolselector®2 User Guide | Russian | Russia | 25 Feb, 2020 | 4.4 MB | |
User guide | Coolselector®2 User Guide | Chinese (CN) | Switzerland | 04 May, 2020 | 25.2 MB | |
User guide | Coolselector®2 User Guide | French | France | 05 Mar, 2020 | 5.5 MB |
Videos
Training videos
Our training videos are constructed to give you an introduction to each of the main areas of Coolselector®2. The videos show examples of use cases as well as useful tips and tricks for every day use.
Recorded training sessions
Whiteboard sessions
Learning