• My Apps
    My Apps You will have the option to use My apps once you login.

Europe’s first hybrid-powered heavy truck

Friday, May 25, 2018

Electrifying heavy duty trucks

Sisu is a Finnish truck manufacturer that makes vehicles for standard road transportation applications. Also for specialized applications such as the Finnish Defence Forces. Sisu trucks can be factory customized for a variety of applications. For example, they can be configured as a timber lorry, or with a plow mount in the front. There are several configurations for hydraulics, such as tipping and tailgate.

Sisu manufactures a few hundred diesel-powered trucks every year. The company set a target for 20% of all new trucks to be made with a hybrid drivetrain by 2019. Providing new functionalities, lower fuel consumption and higher performance to customers. This could further speed up the breakthrough of the hybrid system.

Tackling fuel consumption with minimal changes

The main challenge for Danfoss was to develop a solution that reduced fuel consumption (and therefore lowered emissions). At the same time, making minimal changes to the truck itself. The solution also needed to be compatible with the existing drivetrain and easily integrated into the truck's electrical system.

Bringing together diesel and electrical power

Danfoss developed the electric power system including parallel hybrid drive for a proof of concept vehicle. Power is provided by an electric motor and a diesel engine connected via the same axle.

The electric motor assists the diesel engine during peak load demand from the drivetrain. In addition, it charges the supercapacitor energy storage unit during off-peak periods. The electric motor is located between the engine and gearbox. This ensures simple assembly with no need to alter the existing chassis or suspension structure.

Danfoss developed the electric drive system to work in parallel with the Mercedes-Benz OM471 and OM473 diesel engines. The technology from the proof-of-concept unit has since been adopted for use in the Sisu Polar Hybrid truck range.

Improved fuel efficiency, fewer carbon emissions

Danfoss developed a solution that lowers fuel consumption and emissions. In addition, the powerful hybrid system boosts available low speed torque. This means the driver experiences the sensation of power when the vehicle is accelerating.

With the electric drive system, the driver feels the impact of the torque immediately, even at very low speeds. This makes the electric machine a useful addition to any powertrain. It improves on the performance capability of a combustion engine.

The solution also enables the use of the vehicle with or without a source of electric power. For instance, the system can be fully automatic or manual. Since the drive line is mechanically continuous from the diesel engine to the axle. The system supplies additional power and charging automatically, which means the driver can better focus on the road. The driver can also keep track of the system’s data. If required, bypass the automated system and take control.

In manual mode, the driver can use the electric motor to rock the truck back and forth if conditions are muddy. In addition, he can make a three-point turn without having to shift gears from forward to reverse. The same movements can be done quickly and easily using a separate joystick-type controller. This is enabled by the location of the clutch between the combustion and electric machines in the drivetrain.

Since the successful delivery of the first proof of concept vehicle Sisu has received orders for several hybrid trucks. The first is scheduled for delivery in Autumn 2018.

Danfoss Editron

Danfoss Editron

Danfoss Editron is taking fuel savings and energy efficiency to the next level. We specialize in hybrid and electric powertrain systems for marine, off-highway and commercial transport markets. Our mission is to end pollution through electrification.