Electric Heating by Danfoss chosen to protect XVIII-century baroque palace in Kyiv

Wednesday, October 7, 2020

Designed by Bartolomeo Rastrelli in the second half of the XVIII century, Mariyinsky Palace is the official ceremonial residence of the President of Ukraine used for hosting other heads of state.

Electric Heating by Danfoss was chosen as sustainable modern technology to protect the historical landmark during its reconstruction.

Solution:

To ensure safety of visitors, an efficient ice and snow melting was needed in the outdoor area surrounding the palace. Two flexible electric heating system were used. They perform effective protection of surface meanwhile defending environment against salting and antifreeze damages.

The outdoor electric heating system is fully flexible and functions automatically: it is switched on once the sensors detect low temperature and moisture, and switched off after the surface is cleaned. This provides a cost-effective protection to the large area being most energy efficient solution for the ground ice and snow melting applications. Managed by the high-end controller, the system is maintenance free.

Result:

The ceremonial residence of the President of Ukraine is equipped with “Around the Clock” snow cleaning service by Danfoss. Mariyinsky Palace is open for public excursions from September, 2020.


Project Overview:

Installed power: 250 kW
Products: ECsnow 30T - 230V 8.4 km; ECtemp 850 controller
Year of implementation: 2016


Facts about Danfoss Electric Heating:

Electric Heating by Danfoss is energy efficient and environmentally friendly meeting your needs in various applications. It enables you great comfort and convenience whilst ensuring user friendly solutions with lasting effect and highest quality standards.

Electric heating solutions are supported by legislation in key European countries. Directives that are coming in force in the biggest European markets give the green light to the trend: use eco-friendly systems and new materials ensuring energy saving.