Aims to achieve a carbon neutral, circular and climate adaptive campus by 2030. One of the keys to realizing this ambitious goal is the university’s geothermal project, which will provide sustainable heating to both the campus and approximately 6,000 households in Delft. The project has been linked to a scientific research program, studying the use of geothermal energy in an urban environment. TU Delft partnered with Danfoss to prepare the campus’ infrastructure for the transition by installing new, efficient heat substations.