Poultry and livestock products are big business in Pennsylvania, responsible for $4.5 billion in annual agricultural sales. Organic poultry farmer Earl Ray Zimmerman is adding to that number thanks to an innovative heating system utilizing Danfoss AB-QM™ Pressure Independent Temperature Control and System Balancing valves to maintain the precise temperatures chickens need to keep gaining weight to go to market as fast as possible.
“Chickens are affected by temperature,” observes Matt Aungst, co-owner of Total Energy Solutions, a Willow Street, Pa.-based firm that engineered the heating system. “A change of just a few degrees affects the birds’ eating habits. And if they don’t eat, they don’t put on weight. Missing the growth schedule for thousands of birds for just one day stretches a farmer’s time to market and cash flow, something poultry producers want to avoid at all costs.”
Precise temperature balancing is critical in each of the 45-by-500-foot houses Zimmerman uses for broilers, chickens specifically raised for meat production. “Each building is wide open,” Aungst describes. “So each area has a different heat loss profile depending on the location in the building. The goal is to keep the entire building at 93°F at the beginning of every flock.”
To hit that goal, Aungst and his partner John Albright offer an air handler designed specifically for chicken houses. Called the CUBO series air mixer, the system uses a centrifugal fan to circulate air through the mixer’s coil into the chicken house to maintain even temperature throughout the living area. Each building employs eight CUBO units suspended from the ceiling. A heating coil in each unit is supplied by a hot water circuit regulated by its own Danfoss AB-QM™ valve.
AB-QM™ valve enables precise temperature control
“The AB-QM™ valve is a pressure independent control valve (PICV) that provides just the right flow of hot water to satisfy temperature requirements exactly, which is ideal for our system,” says Aungst.
On warm days, the CUBO mixer pulls hot air from the ceiling level and expels it in a 360-degree circular flow just above the floor to eliminate stratification.
On cold days, a boiler supplies hot water to the internal heat exchanger inside each CUBO unit. The system engineered by Total Energy Solutions uses an unusual fuel source – dried chicken waste – to fire the 1.5 million BTU boiler, which can handle 100 percent of the heat load.
“The water flow to each coil is based on the heat load," explains Aungst. "At full load, the system supplies 180°F water at 11 gallons per minute (GPM) to each CUBO unit. But conditions seldom call for that much heat."
That's why Aungst is using Danfoss AB-QM™ valves. Eight AB-QM™ valves are located along the main piping circuit that runs near the peak of the roof in each building. One valve is used to control the water flow to one coil. The valve increases or reduces the flow of hot water supplied to the coil depending on whether the zone temperature sensors call for more or less heat. Because 100 percent flow is usually not needed, a Danfoss variable frequency drive (VFD) incorporated into the circulating pump motor can reduce pump speed as flow is reduced, which cuts electricity consumption.
Related products
-
if (isSmallPicture) {
; } else if (isBigColumns) {
} else {
}
AB-QM™ Pressure Independent Balancing Control ValvesSimple Affordable Comfort - Pressure independent control excellence from the global market leader for over 30 years. Discover how Danfoss AB-QM™ Pressure independent balancing control valves (PIBCVs) can improve system efficiency by eliminating overflows and increasing ΔT.
Danfoss offers a complete range of innovative solutions - ½" to 10", to meet your HVAC system's needs for optimal flow control.