Reduced installation and running costs in chillers
Core component of the HVAC system, a chiller cools the water or brine used to cool and dehumidify air in buildings or industrial processes. It's a factory-assembled unit that cools the water or brine using an evaporator, and has an internal or a remote condenser with appropriate controls. The condenser can be either water-cooled or air-cooled. A chiller based on such a design has a variety of applications, from space cooling to process purposes.
A typical modular chiller unit uses tandem fixed-speed compressors to provide some part-load capability for the modular system. These units share the same water system to provide cooled or heated water to the building.
Danfoss offers the option of using only one variable speed compressor instead of a fixed-speed tandem in order to better match the capacity requirement of the modular chiller unit.
Why choose Danfoss variable speed compressors for modular chillers?
For the end user:
- Using the Danfoss inverter compressor solution, the unit will have much better seasonal energy efficiency, providing energy savings all year round. The energy saving potential in both heating and cooling modes is illustrated in the graph below as a function of ambient temperature:
For the OEM:
- By using one inverter compressor, the design of the unit can be simplified to provide continuous capacity output over the full speed range. The manufacturer can provide flexible options to the end user such as:
- Full variable speed solution, where all units use variable speed compressors to achieve the best efficiency and modulation.
- A solution using a combination of variable-speed compressors with other fixed-speed compressor modules, allows a good improvement in energy efficiency whilst remaining cost competitive.
- Cost reductions can be achieved because fewer components may be needed, such as multiple fixed-speed compressors, relays, and pressure switches; the amount of piping required will also be less.
- Modular chiller units using Danfoss variable speed compressor solutions also provide the opportunity for manufacturers to offer an alternative to VRF units.
- VZH variable speed chiller designs also give manufacturers the opportunity to offer innovative and differentiated solutions which can improve product and brand image, instead of units using traditional on-off compressor technology.
What other benefits are there for your customers when they choose Danfoss inverter compressors?
- Reduced installation costs: thanks to the more reactive adaptation to cooling demand, the manufacturer or the installer has the possibility of eliminating or downsizing buffer water tanks, with a significant cost saving and reduction in footprint
- Lower sound level: under part-load conditions, especially during the night, chillers using a variable speed solution will have lower sound levels than traditional on-off compressor systems in both running and start-up periods
- Short pay-back period: the pay-back period with this innovative technology can also be as little as 2 years for the end customer
- Lower environmental impact: reduced impact on the environment with R410A refrigerant
The most important benefits for customers
- Energy savings
- Reduced installation costs
Case studies
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Engineering the precise indoor comfort for the better movie experienceLearn how Danfoss offered a solution for a plug-and-play, maintenance-free HVAC system which is convenient and efficient, and delivers precise temperatures, helping PVR deliver a truly world-class movie-watching experience to its customers.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Delivering Smart Indoor Comfort to the world’s 1st Solar Powered AirportAirports globally have evolved from just being docking stations for the flights to becoming an avenue that houses the best experiences a traveler can get. From retail stores to restaurants, from lounges to culture showcase centers, every new airport today is pushing the standard on experiences. But, delivering these uber experiences alongside a thermal comfort inside the airport expends a lot of energy. With close to 100 million passengers travelling through domestic routes every day in India[1] and with the number exponentially increasing, curating a comfortable experience for the guests can be a challenge.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Driving the Metropolis with an Energy-Efficient MetroDanfoss offered its energy efficient solutions to Delhi Metro to save energy without compromising on the indoor comfort and convenience of its commuters and is committed to doing so in future. Driven by a deep application expertise and future-facing technologies, Danfoss is poised to support the metro to be energy-efficient and to yield high performance, and thereby engineering tomorrow’s India, today.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Denmark's new climate-friendly hospitality giant depends on Turbocor® oil-free chillerThe new Alsik hotel in Southern Denmark sets a higher standard in energy-efficiency and is built to reach 76% CO₂-neutrality. A main contributor is the 900-kW chillers by Clint (a company of G.I. Industrial Holding) which features award-winning Danfoss Turbocor oil-free compressors.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Oil-free compressors maintain consistent performance over timeDanfoss conducted a study to see how long term operation affected performance on Danfoss Turbocor® compressors. The results showed that oil-free, magnetic bearing compressors maintained consistent performance even after 10+ years of operation.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Research laboratoriesRenovation of Key Laboratory in Shanghai illustrates the benefits of temperature control and energy savings in critical applications with inverter technologies
Contact us
For further information, please contact us.
Highlighted products
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Inverter scrolls - VRJDanfoss inverter scroll compressor solutions for commercial air conditioning and process-cooling applications. R410A, single units. VSH: first-generation commercial inverter scroll compressors with frequency converter CDS302. VZH: second-generation commercial inverter scroll compressors with frequency converter CDS303. VRJ: first high-tier residential inverter scroll compressors with frequency converter CDS801.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Turbocor® - TTDanfoss Turbocor® model TT oil free compressors are available in four different models ranging from 60 tons to 200 tons / 200 to 700 kW utilizing R134a or non-flammable, low GWP R513A.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Inverter scrolls - VSHDanfoss inverter scroll compressor solutions for commercial air conditioning and process-cooling applications. R410A, single units. VSH: first-generation commercial inverter scroll compressors with frequency converter CDS302. VZH: second-generation commercial inverter scroll compressors with frequency converter CDS303. VRJ: first high-tier residential inverter scroll compressors with frequency converter CDS801.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Reciprocating inverter - VTZDanfoss reciprocating inverter compressors avoid oversized and short cycling systems. The compressor automatically adapts to the current load. By combining an efficient Danfoss Maneurop® reciprocating compressor with a Danfoss Drive, the company provides an innovative and intelligent package that utilizes variable-speed technology to ensure superior efficiency across the entire operating range for precision cooling.
-
if (isSmallPicture) {
; } else if (isBigColumns) { } else { }Turbocor® - VTTDanfoss Turbocor® model VTT oil free compressor is available with a capacity up to 400 tons / 1430 kW using R134a. This compressor is designed for water and evaporative cooled chiller applications.