Saving energy

Control your room heating and costs
With energy prices on the rise, homeowners and renters alike are hunting for ways to reduce energy consumption and save money.
Control your heating costs
Your home is your most important environment – this is the place where you eat, sleep, relax and raise your children. Therefore, it is highly important that you have the best possible room comfort without constantly adjusting your thermostats. Not only will you have optimal room heating, you will also reduce unnecessary energy costs.
It is important that your radiator thermostat is free to measure the real temperature of the room. Here we have compiled top tips to help you to get the greatest efficiency out of your home thermostat.

Tip #1: Comfort and energy savings
Equally and comfortably distributed heating makes it possible to lower the room temperature and still feel warm. For every degree the room temperature can be lowered, 5% energy is saved.

Tip #2: Use all radiators in the room
Set the temperature control on all thermostats in the same room to the same level. You’ll save nothing by turning one of your room thermostats down or off. The other radiators will have to work harder at heating your home, resulting in poorer heat distribution.

Tip #3: Don’t cover or block your thermostat
Never cover or block your thermostat with items that may disrupt an accurate room temperature reading. These items may include clothes, curtains or furniture placed either over or in front of the thermostat.
The temperature around your thermostat should be the same temperature as in the rest of the room, so keep the air around it flowing freely.

Tip #4: Set the levels and leave them alone
Constantly adjusting your room thermostats will not save energy … or money. Set the thermostats to your desired level and let them control the room temperature on their own.

Tip #5: Turn off during ventilation
Shut down all the thermostats in rooms where ventilation is required. Leave the windows open for 5-6 minutes. When you’re finished airing out the room, turn the thermostats back to the same setting that they were on prior to turning them off. If you don’t turn down your thermostat, it will react to the drop in temperature by heating automatically.

Tip #6: Regulate humidity levels
It’s a good rule of thumb to air your rooms out every day – rain or shine. The humidity levels in the home should be no more than 40-50 percent.

Tip #7: Lower the temperature during night
You can save energy and money by turning your radiators down 2-3 degrees at night. At 17°C you will also ensure yourself a better, healthy sleep. But remember: If you turn them down more than 3 degrees, the money you could save will be used on reheating the room again.

Tip #8: Maintain ideal thermostat temperature throughout day and night
Optimal temperature during the day should be around 21°C and 17°C at night. Even if you want to go lower with rooms that you don’t use often, always maintain a minimum of 14°C as it can result in building damage, dampness, condensation, and mould.

Tip #9: Location is key
To ensure that your thermostat [GA1] works as effectively as possible, it is important to carefully consider where you place it. A good location would be an interior wall, and ideally mounted about 1.5 metres above the floor. This means that it will receive a more accurate measurement of the room’s condition and would ultimately result in the radiators delivering a more desirable room temperature.
Remember to keep your thermostat out of direct sunlight to ensure a more accurate reading.

Tip #10: Room-by-room comfort
At Danfoss, we have a saying: Real room comfort is when you’re not aware of the temperature. That is exactly what our thermostats enable you to achieve. You can schedule your desired temperature for any time of the day or night – room by room – to suit your family’s everyday routine … all while saving energy and money.

Tip #11: Replace after 15 years
If your thermostat is more than 15 years old, it needs replacing. Our complete range of energy saving home thermostats are the best thermostats on the market and are specifically designed to meet all of your home heating needs.

Tip #12: Lower the temperature when travelling
If you leave your home for a long period of time you need to lower the temperature to save energy.
Our smartheating programmable thermostats can be set to frost protection or scheduled to enter AWAY mode when you’re on holiday for optimal home energy efficiency.

Tip #13: Go wireless
Today, a wireless room thermostat is a very popular way to go. We offer a wide range of wireless, programmable thermostats that can automatically adjust the room temperature when needed.

Interested in more tips and advice?
From simple upgrades to more advanced smart heating of your home, Danfoss products and solutions can help you take control of your heat consumption—whatever your heating bill is up against.