A good example of this need for cooling during manufacturing is found in the plastics industry, where injection machinery heats the plastic polymer to enable it to be moulded or extruded. In the blow moulding of plastic films, the temperature control of the extruded film is important, since this affects the quality and thickness of the film.
Cooling equipment can be of different types, depending on whether air or liquid is the cooling medium which needs precise temperature control. The cooling equipment often needs to be very flexible in order to allow industrial machinery to use the same cooling equipment in different processes. For example, a plastic film blow-moulding machine can produce thin films; then the temperature set point needs to be relatively high (typically 20°C). The same machine can also produce thicker plastic films, but then the temperature set point needs to be lower.
In addition to the need to be able to maintain different temperature set points during a manufacturing process, process coolers have to be able to maintain a stable temperature at the set point despite variation in the ambient temperature.
Why choose Danfoss variable speed compressors for process cooling?
By using the Danfoss inverter compressor – a reliable compressor combined with a prequalified drive – the challenges involved in manufacturing applications like the above can be met.
Variable speed solutions adapt very quickly to cooling demand and keep the process at a precise set point (±0.2°C) despite varying ambient temperatures. If process parameters need to be changed, smooth and very precise temperature control is possible, as shown below in a comparison between close control using inverter compressors and using traditional on-off compressor technology.