A unique supermarket
On June 29th the COOP 365 Smart Store opens for the public for the first time. In the Danfoss Smart Store the cooling and heating technologies are in operation 24/7. It’s not a laboratory simulating real-life operation. Customers open cabinet doors hundreds of times a day and every time it puts demand on the cooling and heating of the supermarket. The Danfoss Smart Store demonstrates our available solutions in action.
BALS, Brugsforeningen for Als and Sundeved, Denmark’s largest independent supermarket association, will rent the building from Danfoss and will install a COOP 365discount supermarket. BALS, which works together with COOP, has a total of 13 stores in the area around Sønderborg in Denmark and since 2015 has consistently reduced the consumption of energy in its stores. So far, they have cut 44 percent of their total CO2 emissions. Therefore, it was a natural next step that BALS became a partner in the project.
Lars G. Andersen, managing Director of BALS, says:
“We already have a lot of experience, but the energy price spikes have put further pressure on the need for change. Our 13 supermarkets have been modernized, and we have nearly no cost for heating in the stores because the heat comes from our freon-free refrigeration systems, solar cells, and heat pumps. It is an advantage with the current energy prices, and it reduces our CO2 emissions. We are proud to be part of one of the most energy-efficient supermarkets in the world and test the solutions that can help buildings become climate neutral.”

New ‘Smart Store’ paves the way for 21st century supermarkets
New “Smart Store” will work as Danfoss’ test center for energy efficiency technology. ‘The Smart Store’ is expected to be approximately 50% more energy efficient compared to a typical supermarket with a first-generation CO2 refrigeration system.
Learn more
Scalable technologies
The installations and technologies in the supermarket are scalable. They can be applied in the smallest store up to the biggest hypermarket.
The supermarket cooling (refrigeration and comfort cooling) systems run exclusively on natural refrigerants (CO2). CO2-based refrigerants do not deplete the ozone layer and have the lowest possible Global Warming Potential (GWP) score. In addition, CO2 refrigerants outperform traditional HFC-systems when it comes to energy efficiency in different weather conditions.
The supermarket is equipped with a heat recovery unit capturing excess heat from the cooling systems to provide space heating for the entire store as well as the surrounding community through the district heating network. The heat recovery unit, can by re-using the excess heat from the cooling system, reduce the external heat requirement with up to 89,7%. Furthermore, the energy pack can supply additional heating and cooling when needed.
Smart energy systems applied
100 KW solar panels on the roof help to optimize store operations. On sunny days, solar energy can be accumulated in the freezers. Turning the temperature in the freezers further down from e.g., -18 to -25 help accumulate solar energy ( while reducing battery storage). When the solar panels are less efficient due to no sun the temperature rises back to normal settings.
Co-developing with customers
The supermarket has two separate refrigeration systems installed that run independently of each other. Therefore, operations of a supermarket continue while Danfoss co-develops new solutions with customers. And when future applications are being tested, the cooling cabinets and freezers stay cool.
Certifications
-
DGNB Gold (EU)
-
LEED Platin (USA)
The final certifications can only be obtained after six months of operations.
The Smart Store provides inspiration for building DGBN / LEED certified supermarkets showcasing that it does not require a lot of extra resources to ensure that the building is healthy, future proof, and positively impacting the surrounding community.
Biodiversity
In order to positively impact the local biodiversity several initiatives have been taken. Very visible mega pergola surrounding the building which will be watered by use of collected rain- and surface-water. Also, different native grasses as well as a ‘green roof’ will be planted to create a micro-environment for biodiversity.
Cooling and heating capacity for 1,500 m2 store and 250 m2 ADC
-
30 kW medium temperature
-
13 kW freeze - low temperature
-
20 kW comfort cooling/ventilation for store and ADC (additional 20 kW from roof-top chiller)
With the world’s population expected to reach 10 billion people by 2050, sustainable food retail and storage are more important than ever. Yet this is an often-overlooked step in the decarbonization of society.
Read full case story

Case studies

A busy Danish supermarket reduced its annual heating bill by 89.7% and its CO₂ footprint by 6.7 tons a year by making use of the waste heat from its refrigeration system.

Globus had an ambitious target: to open the new 25,000 square meter hypermarket using transcritical CO2 for its refrigeration and heating. Danfoss helped KrioFrost—a Moscow-based refrigeration equipment producer and installer—to equip Globus’ huge new store in the Moscow suburb of Salaryevo with the company’s first transcritical CO2 booster refrigeration system.

The supermarket aktiv & irma in Oldenburg, Germany, has pressed the start-button to a solution enabling it to store and generate electricity. The grocery store’s manager calls it a leap forward in energy supply. Danfoss and SMA have helped make it happen. Learn how.

Danfoss offers a complete portfolio of gas and liquid ejectors that provide significant benefits in CO2 refrigeration applications. Here we take a closer look at these offerings: the Multi Ejector Low Pressure (LP), the Multi Ejector High Pressure (HP), and the Liquid Ejector (LE). All three ejector products are only available as a complete Multi Ejector Solution™ where the ejector is bundled with the AK-PC 782A pack controller to provide the robust system controls necessary for efficient and reliable operation.

Danfoss has pioneered two control algorithms that help you achieve this balance. The Minimum Stable Superheat (MSS) algorithm has been an important part of the Danfoss ADAP-KOOL® offering for years and is still the ideal choice for adaptive evaporator control for dry expansion. Now Danfoss introduces the next generation: Adaptive Liquid Control (ALC).
Related applications

Your refrigeration system is the natural place to look for energy efficiency gains. To unlock that potential, you need a controller, expansion valve, and high accuracy sensors that are smart enough to make the technology work together—and a system manager that can help you see and control the bigger picture.

Danfoss has pioneered CO₂ refrigeration systems for more than 10 years. Learn more about our CO₂ refrigeration solutions for supermarkets here.

The Heat Recovery Unit (HRU) is designed to recover the waste heat from C02 refrigeration installations. Recovered heat can be used for own heating purposes or returned to a District Heating Utility network.
Highlighted products

The CCMT is an electric operated valve designed specifically for operation in CO2 systems. The valve is capable of functioning either as an expansion valve, as a pressure regulator for the gas cooler or as a gas bypass valve with back-pressure regulation in trans-critical or subcritical applications.

The system manager is the key component of the intelligent Danfoss ADAP-KOOL® refrigeration system for food retail.

Refrigeration pressure transmitters are used for commercial air-conditioning and for commercial and industrial refrigeration applications. They are made in stainless steel to be compatible with fluorinated and natural refrigerants and laser welding with no soft seals ensure hermetic tightness for decades.

Refrigeration temperature sensors are used for applications within air-conditioning as well as commercial and industrial refrigeration applications. The Pt 1000 sensor element meets the DIN/IES 751 class B requirements and ensures an accurate and reliable temperature signal applicable for regulation, safety and data logging.
Contact us
Want to experience real supermarket efficiency?
Reach out to us if you are interested in visiting our SM ADC and see real live.