These webinars are aimed at engineers working in the field for design, installation or service of commercial refrigeration as the points covered are applicable to many types of installations and focus on both practical and design basics to ensure the system operates correctly and has a good life.

- From Feb 5 08:30-09:15 and 15:00-15:45
The webinar will explain how to make the selection match between the condensing unit and the evaporator to ensure the balance point of the refrigeration system is correct for the application - This will then ensure the correct evaporating temperature and correct relative humidity for the cold room.

- From Feb 09, 09:00 AM
Get an introduction to cold rooms and the role they play in food safety and storage. Application expert John Broughton will walk you through what a cold room is, how it fits into the cold chain, how it is constructed, and the types of refrigeration and control systems that are in use today.

- From Feb 09, 02:00 PM
The cooling industry is changing rapidly. New cold room technologies, regulations, processes, and methods are being introduced all the time. In this session, John Broughton gazes down the road to see what exciting cold room developments lie on the horizon and discusses what cooling professionals can do to get themselves ready for them.

- From Feb 09, 10:00 AM
Learn about the operational challenges that come with building and maintaining a well-functioning cold room. John Broughton will share the typical issues that can arise and, more importantly, how you can diagnose and resolve them.

- From Feb 17th 09:00-09:45 and 15:00-15:45
The webinar will focus on good practices when installing a cold room and the reasons why they are important to ensure the system operates correctly.

- From Feb 09, 10:00 AM
In this new addition to his Cold Room webinar series, John Broughton dives deep into how and why you should defrost a typical cold room (sometimes called a walk-in).
Join John for a quick 30-minute look at how frost builds up on evaporator components, why defrost is needed, and how this affects the operation of the refrigeration system. He’ll also walk you through the various defrost methods in use today and how to set them up including fault finding to ensure the evaporator is always operating effectively.
Ready to optimize your cold room and eliminate frost buildup?

- Mar 3rd 09:00-09:45 and 15:00-15:45 CET
The webinar will focus on good practices when commissioning a cold room and the reasons why they are important to ensure a long and happy life of the components.