Danfoss Solution behind the SIB ZERO+ House, Sonderborg, Denmark

Thursday, September 11, 2014

The SIB ZERO +House is an excellent example of Danfoss' wide range of professional and energy saving solutions put into practice. Danfoss is also an active and leading figure on a market that is increasingly focused on low energy consumption.

The SIB ZERO +House is the name of Denmark's first low energy +house. The house, which was recently completed in the town of Sønderborg, has positive annual energy costs and provides a glimpse of tomorrow's energy efficient home.

The 200 m2 home actually produces more electricity than it consumes on an annual basis, which is why it is known as a +house. The excess energy is created through a unique combination of known technologies that turn the home's energy consumption into energy production. Danfoss contributed with solutions for the indoor climate and comfort system to this project, which includes the use of a Danfoss Air system and Danfoss fast acting floor heating.

One of the secrets behind the low energy +house is effective insulation. However, the well insulated home also requires efficient ventilation in order to maintain a healthy indoor climate. In this case, mechanical ventilation combined with heat recovery was the only real solution. Anything else would have resulted in excess energy consumption.

In order to further optimize energy consumption, Danfoss has combined the ventilation system with a so-called geothermic preheating surface which consists of an 80 meter long pipe in the garden that captures heat in the ground produced by the sun. This energy can then be used to heat the air in the winter months and cool down fresh air in the summer.

Danfoss' energy efficient total solution is perfected by an underground heating pump that heats up utility water and is used for the home's central heating. The heat is emitted via fast acting floor heating that is controlled precisely by a wireless thermostat that uses infrared sensors to measure the floor's surface temperature.

Related products

  • if (isSmallPicture) { Room controls- Danfoss; } else if (isBigColumns) { Room controls- Danfoss } else { Room controls- Danfoss }
    Room controls

    To ensure hydronic (water based) underfloor heating or cooling systems achieve the expected high level of comfort and low energy consumption, good room temperature controls are essential. They control the room or floor temperature to avoid overheating. For optimal comfort each room has it's own room thermostat.

  • if (isSmallPicture) { Manifolds and actuators- Danfoss; } else if (isBigColumns) { Manifolds and actuators- Danfoss } else { Manifolds and actuators- Danfoss }
    Manifolds and actuators

    Danfoss floor heating manifolds are characterized by their flexibility to establish the best suited manifold solution based on requirements. Select from all the components to construct a manifold with or without pre-setting, flow-meters, shut-off valves and air-vents that best fits your project.

  • if (isSmallPicture) { Mixing shunts- Danfoss; } else if (isBigColumns) { Mixing shunts- Danfoss } else { Mixing shunts- Danfoss }
    Mixing shunts

    Danfoss floor heating mixing shunts establish a water temperature low enough to safely be distributed through the floor heating system. It’s designed to fit the FH manifolds and mixes the warm supply temperature with colder floor heating return flow to the required floor heating supply temperature.

  • if (isSmallPicture) { Panels and pipes- Danfoss; } else if (isBigColumns) { Panels and pipes- Danfoss } else { Panels and pipes- Danfoss }
    Panels and pipes

    Danfoss floor heating panels establish the basis for a hydronic floor heating system. The Basic system contains 3 different panel models; BasicClip, BasicRail and BasicGrip. With these you can easy establish a wet (in-screed) floor heating system. For dry systems our SpeedUpTM panels are available.