Rasmus Frederiksen, technical manager at KNI A/S, who has been in charge of the project says: "As we did the project calculations it was very important that what we presented to the board would also be proven possible in reality. With our calculations on payback times of 1½ year we were certain that it would also hold up in reality, but we had not anticipated that it could be as short a period as ½ year, which has proven the case in some places." And he continues: "In our evaluation of alternatives we looked at factors like energy consumption, silent operation and that installation could take place both outside and inside. The installations have run smoothly and our stores and neighbours are very happy with the reliability and silent operation".
The 50 units that have already been fitted now show big economical benefits such as:
- Less energy consumption
- Fewer service visits and through that savings on travel expenses
- Less food los as a result of more reliable units
Rasmus Frederiksen, KNI A/S, underlines the silent operration of Optyma Plus™ with a story of a stores keeper who lived next to the stores who got out of bed several times during the night to check that the unit was till running. The shop keeper was so used to being able the hear the old unit that it took some time to get used to the fact that silence did not mean that the unit had stopped, but just that Optyma Plus™ was so munch more silent than the old unit.
In the perspective of the many advantages KNI A/S is already now very satisfied with Optyma Plus™.
The next step that interest KNI A/S, is the possibility of remote monitoring through ADAP-KOOL®, which is possible with the new Optyma Plus™ New Generation. These units could be interesting for selected shops as it would be possible to handle eventual problems directly from the head office in Sisimut. Further advantages with Optyma Plus™ New Generation are the possibility for further energy savings as they are fitted with a new controller that regulates the crank case heater and fan motor.