Ziyang Budweiser Factory, China
In 2011, the first facilities for production of Budweiser beer in China were established in the Sichuan province. In order to keep pace with the ambitious commissioning plan, the construction period of the refrigeration system for the fermentation area was limited to four months and called for fast design and construction.
To deliver on the tight time schedule, the Danfoss ICF valve stations were chosen for the Ziyang plant. Compared to assembly of traditional components, the ICF solution greatly reduces the time spent on welding. At the same time the reduced number of welds prevents leakage and provides high safety.
According to calculations after the installation of the 178 sets of Danfoss ICF control units, the Budweiser Ziyang factory has achieved savings of 50 % in the installation phase and savings of 30 % for maintenance and operational costs.
In addition to the ICF valve stations in the fermentation area, Danfoss supplied a number of other refrigeration components for de-oxidization, hops storage and icy water control. The applied solutions help Budweiser achieve significant energy savings on its first Chinese plant.