Water and energy loss put pressure on the water industry

According to World Economic Forum 2017, a water crisis is evaluated as one of the highest risks to the world and with the largest impact.

As populations grow, pressures mount and finding a more sustainable relationship between water and energy supplies become critical in less than two decades.

Today, close to one third of the world’s population is estimated to live in water stressed and scarcity areas and by 2040, almost 20 % of all countries are anticipated to experience extremely high water stress.  

Yet, water and energy loss in the water sector are extremely high. In fact, the average amount of water wasted by waterworks is 40 % worldwide and 26 % in Europe – due to errors, leakages, and water pressure. 

At the same time, 4 % of global electricity is consumed by the water industry – a figure that is expected to double by 2040 – and water accounts for up to half of a municipality’s total energy bill.

Water industry challenges

Todays challenges - Danfoss

Today’s challenges Tomorrow’s achievements

The industry challenges reflect a growing need for efficient water supply and treatment.

The good news is that technologies to reduce energy consumption and leakages in all stages of the water cycle – from production and distribution to wastewater pumping and treatment – already exist.

Pressure management is key throughout the water cycle

Global Director at Danfoss Drives Segment, Mads Warming, explains why there is a need for more efficient water supply and treatment on a global scale.

Water treatment illustration - Danfoss

Pressure control is key to reduce water and energy loss

Danfoss pressure sensors and variable speed drives are a key component for reducing water and energy loss throughout the whole water cycle.

Experiences from 112 systems in 10 different countries show that better pressure control reduces non-revenue water and unnecessary energy consumption significantly.

In average, improved pressure management leads to 38 % reduction in pressure and 53 % less new breaks. Among other benefits, the energy consumption is reduced by 20-40 % and the typical water leakage reduction is 38 %. Moreover, the improvements result in extended asset lifetime and fewer network related complaints.

Danish water utility sets new standards for sustainability

The Danish water utility, Aarhus Water, is running with only 6 % leakage. Danfoss has contributed through the whole water cycle.

Water and waste water - close up - Danfoss

Bringing water and energy use into balance

The increasing global demand for water and energy has put immense pressure on both industries to find a path towards a more sustainable future. And pressure itself is the key to achieving this goal.

Related products

  • VLT® AQUA Drive FC 202
    VLT® AQUA Drive FC 202

    FC202 drives and controls all types of pumps and comes equipped with a cascade controller.

  • KP / KPI, pressure switches for light industry

    Danfoss KPI pressure switches are used for regulating, monitoring and alarm systems in industrial applications. The KP series are suitable for plant in connection with liquid and gaseous media.

  • MBS 1900 - Danfoss
    MBS 1900, pressure transmitter for air and water applications

    The pressure transmitter MBS 1900 is designed for use in air and water applications like booster pumps and air compressors. The flexible pressure transmitter programme covers different output signals, absolute and gauge (relative) versions, measuring ranges from 0-4 bar to 0-25 bar and a wide range of pressure and electrical connections. Enclosure material is stainless steel AISI 316L.

  • MBS 3000 series - Danfoss
    MBS 3000 series, compact pressure transmitters

    The compact pressure transmitter MBS 3000 is designed for use in almost all industrial applications, and offers a reliable pressure measurement, even under harsh environmental conditions.
    The flexible pressure transmitter programme covers all standard output signals.

  • MBS 1700 - Danfoss
    MBS 1700 semi-flexible pressure transmitter

    Pressure transmitter, type MBS 1700 is designed to a variety of applications and easy installations within the distributor market. The transmitter offers highly reliable pressure measurement, ensuring that even the slightest change is detected immediately.

Videos

Case studies

Marselisborg Aarhus - Danfoss case

The worldwide first energy-neutral catchment area

The Marselisborg catchment area in Aarhus has achieved 100 % energy surplus production - by minimizing consumption throughout the whole water cycle and maximizing energy production from the wastewater facility.

Articles

  • AEL Intelligent Blasting cuts energy consumption by 500 kWh per hour
    AEL Intelligent Blasting cuts energy consumption by 500 kWh per hour

    This 720 Mtpd nitric acid plant in South Africa saves 3.6 M Rand annually on operating costs, thanks to to VLT® drive control of electric pumps and motors.

  • Seawater
    Creating a sustainable future with seawater

    Over the past decade, the use of Sea Water Reverse Osmosis (SWRO) for desalination has taken off. With proven efficiency rates up to 92% and energy savings of up to 65% compared to traditional solutions, the opportunities of SWRO technologies deserve further exploration.

  • Global study: Pressure management reduces water and energy loss Danfoss
    Global study: Pressure management reduces water and energy loss

    Throughout the entire water cycle, pressure plays a key role in ensuring an efficient, reliable, and sustainable water supply. And for decades, the water industry has struggled with numerous pressure-related challenges in the water system. By using intelligent pressure and flow management, a global study proves how water facilities can reduce unnecessary water and energy loss.

  • A world of water under pressure Danfoss
    A world of water under pressure

    Water puts pressure on people everywhere – whether they are struggling with too much, too little, or too dirty water. In fact, a water crisis is evaluated as one of the highest risks to the world and with the largest impact, according to the World Economic Forum. In this article, we outline the causes of this global water crisis – and offer a lifebuoy that can help us overcome it.

  • Decoupling water from growing energy consumption Danfoss
    Decoupling water from growing energy consumption

    It takes water to produce energy – as it takes energy to produce water. The mutual dependence of water and energy and the accelerating demand for both have a major global impact on economic growth and societies everywhere. To create a more sustainable future, we need to decouple the water industry from growing energy consumption.

  • Tackling non-revenue water with better pressure control Danfoss
    Tackling non-revenue water with better pressure control

    Non-revenue water has been a hot topic in the water industry for years. And for a good reason. In addition to the environmental consequences, non-revenue water has a major impact on the financial viability of water utilities due to water loss and unnecessarily high operating costs.

Contact us

For further information, please contact us.