New TXV Superheat Tuner app helps installers save their customers money

Tuesday, August 21, 2018

Here at Danfoss, we’ve made it our mission to support our customers with the tools and knowledge they need to get the job done quickly and get it done right. We’re with them every step of the way, ensuring that they can deliver best-in-industry service to their customers and maintain long-lasting business relationships.

With that in mind, we’re pleased to announce the release of our new mobile app, TXV Superheat Tuner — the latest in a long line of digital support tools, known collectively as the Danfoss CoolApps Toolbox, all of which can be accessed directly on your smartphone.

With TXV Superheat Tuner, installers can take the guesswork out of their superheat adjustments, cutting service time down to just 15 minutes, rather than several hours. With the app in hand, they will be able to optimize superheat with just one or two adjustments on most thermostatic expansion valves.

Using TXV Superheat Tuner is easy. Installers can enter some basic information about the system they are working on, and the app provides valve-specific adjustment information. Using this information, a service tech can boost the system’s energy efficiency far beyond normal parameters, saving their customers money on their monthly energy bill.

TXV Superheat Tuner uses a set of advanced algorithms to make optimization recommendations. These algorithms, developed by some of our best engineers, take multiple factors into consideration, beyond the basic sensitivity of each valve.

Gone are the days of performing trial and error adjustments. Superheat Tuner helps installers make the best superheat adjustments right from the start, saving time and delivering a better result.

Download TXV Superheat Tuner for free now on your Android or iOS mobile device.