Danfoss solutions for commercial refrigeration approved for use with alternate refrigerants R448A, R449A and R452A

Monday, June 18, 2018

The refrigerant transition is accelerating and HVAC-R associations are urging the industry to move away from R404A. In order to help our customers keep pace, Danfoss has released many product types for the major low-GWP refrigerant alternatives — such as R448A, R449A, and R452A — and continues to update Coolselector® on a monthly base.

Danfoss encourages commercial refrigeration professionals not to delay their switch to low GWP any longer – and pledge to support them every step of the way. Uncertainty over the refrigerant selection and future supply, as well as misunderstandings about component suitability, could be preventing some from gaining the skills and knowledge they need to tackle new refrigerants with confidence.

Danfoss is, therefore, publishing a series of online resources, to help with selection, installation and retrofitting, and has committed to continue to develop qualified components compatible with promising new refrigerants as they arise. It is also introducing a growing number of multi-refrigerant units, to give maximum flexibility both now and in the future.

For small and medium-sized commercial refrigeration applications such as cold rooms, R448A, R449A, and R452A are excellent alternatives to R404A, in complement to R407 A/F. Given the short lifespan and cost of R404A, transitioning to alternative refrigerants having a lower GWP level is a logical step to take now. The solutions are available today for all the parts of the cooling systems with compressors, condensing units, heat exchangers, electric and thermostatic expansion valves, solenoid valves, controls, electronic controllers and other line components – for either low or medium temperature applications. Recent releases include EVR v2, TE5-55, TU valves, MLZ, VLZ, and MTZ scroll and reciprocating compressors, and the Optyma™ packaged condensing units with R448A, R449A, and R452A.

The qualification plan encompasses R513A and R450A* as complementary refrigerant alternatives to R134a as it delivers similar performance.

For self-contained applications typically used in foodservice, the long-term solutions are drawn to natural refrigerants. For applications with a refrigerant charge of less than 150 g, Danfoss offers a wide range of components suitable for various A3* refrigerants such as R290 and R600a. In complement to R404A, R513A is a good option when the charge limitation is over 150g, or when A3 class refrigerant* is not applicable.

Cool Tools:

To help identify components suitable for new refrigerants the best option is Coolselector® 2. The software can make suggestions, allowing users to select the most suitable components based on several parameters such as cooling capacity, refrigerant, evaporation and condensation temperature, plus many other critical variables of common refrigeration systems. In addition to a host of refrigerants, Coolselector® 2 also supports calculations for various refrigeration systems and component selection for cold rooms.

The selection software works hand-in-hand with the Low-GWP tool and the Refrigerant Slider app, allowing customers to easily identify the right components for alternative refrigerants, given their specific thermodynamic properties.
*depending on models

Your toolbox: