Solutions ready to meet global water challenges

Aarhus-Water_wastewater-facility Lack of water and climate change are among the top 5 global risks, according to the World Economic Forum. However, pioneering solutions that can help meet both challenges are ready to be replicated.

- Monday, 24 August 2015 By Danfoss

As the world population rises and people pursue higher standards of living, more water is needed in homes and for production of food and products. By 2050, the United Nations projects global water demand to increase by 55%. However, fresh water supplies are limited, and groundwater is used much faster than it is replenished. In just 10 years, 50% of global population is expected to live in water stressed areas. The increasing demand for water also leads to growing energy consumption, which affects the climate. 

Danfoss has solutions which help countries and municipalities worldwide save water and energy within water supply, wastewater treatment and irrigation of farming areas. For example, Danfoss has supported Denmark in becoming one of the pioneering countries in the water and energy field. The country has grown its economy by 80% since 1980, while reducing water consumption by nearly 40%, and keeping energy use at the same level. Structured water management and innovative technologies have contributed to this decoupling of economic growth, water consumption, and energy use. 

In municipalities, water and wastewater facilities account for the largest consumption of electricity, typically 25-40% of the local authorities' total power use. In the Danish city of Aarhus, a local water company has managed to transform a wastewater facility from being just a wastewater plant into also functioning as a combined heat and power plant, delivering an energy surplus. The plant produces 90% more energy than it consumes. This is feasible thanks to advanced process optimization and by using more than 140 variable speed drives from Danfoss as control handles on almost all rotating equipment. Done optimally, this also creates the maximum amount of sludge and carbon. In a digester, it is transformed into gas used for both electricity and heat production. 

Mads Warming, global director of water and wastewater in Danfoss, says: “It’s a ground-breaking innovation case that shows what is possible within advanced process control. As far as we know, no other country has managed to get a water treatment plant to actually produce so much additional energy based on normal household wastewater. Scaled up, it means that the huge energy consumption from water and wastewater facilities could be avoided, turning the single largest electricity consumer in municipalities into an energy-neutral party.” 

Globally, focus on the high energy consumption in the water and wastewater cycles is also increasing and local regulations are starting to further the use of energy-efficient solutions. One example is EU’s Ecodesign Directive. In the US, the Department of Energy is also proposing minimum efficiency regulations for clean water pumps. Regulations like these are necessary to speed up the realization of the enormous potential. 

When it comes to water supply and irrigation of farming areas, another huge potential is the reduction of water losses in pipework due to leakage. According to the international consultancy firm McKinsey, 167bn USD is wasted every year due to leakage in cities around the world. The United Nations highlights that leakage rates of 50% are not uncommon in urban distribution systems. However, leakages can typically be reduced by 30-40% using technologies like variable speed drives and sensors, which control the pressure in the pipes to avoid water flooding out of holes. At the same time, the drives typically save 20-50% energy.

Mads Warming says: “The global water and climate challenges are a difficult code to crack, but the solutions that can meet them are ready and we also see that focus on leakage reduction and energy efficiency is increasing. Last year, we experienced double-digit growth in our water and wastewater business, and the positive trend continues.”

Besides saving water and energy in countries and municipalities, Danfoss is also helping produce drinking water in remote locations like islands, drilling platforms, and cruise ships. Here, Danfoss takes part in turning seawater efficiently into drinking water using advanced high pressure pumps and energy recovery devices for desalination systems. The Danfoss solutions save up to 50% energy, which is important for the deployment, because at least 70% of the total costs in desalination systems are related to energy use. 

Mads Warming says: “Earlier this year, the World Economic Forum ranked water crisis and failure of climate change adaption among the top 5 global risks and encouraged decision-makers worldwide to take collective action to address them. And there is no reason to wait. Well-proven solutions, which meet the water and climate challenges, are ready and they are paid back fast.”

 

For more information

Danfoss Media Relations
+45 70 20 44 88

Engineering the world of Tomorrow

Danfoss engineers advanced technologies that enable us to build a better, smarter and more efficient tomorrow. In the world’s growing cities, we ensure the supply of fresh food and optimal comfort in our homes and offices, while meeting the need for energy efficient infrastructure, connected systems and integrated renewable energy. Our solutions are used in areas such as refrigeration, air conditioning, heating, motor control and mobile machinery. Our innovative engineering dates back to 1933 and today Danfoss holds market-leading positions, employing more than 26,000 and serving customers in more than 100 countries. We are privately held by the founding family.

 

Be social Take part

Want to socialize with us?

Get to know us and take part in the conversation