Categories
> Refrigeration and A/C
> VLT® Drives
> Industrial Automation
> Heating
> High-Pressure Pumps
 
 
 
 
 

EV220B (15-50 series), Servo-operated 2/2-way solenoid valves

22 Item(s)

FAQ

  • Are the code numbers of the EV220B solenoid valves the same as the previous EVSI valves?
  • Can I use the EV220B with chlorine?
  • What is the difference between the EV220A and EV220B solenoid valves?
  • Can I use the EV220B solenoid valves for steam applications?
  • I need an EV220B 1/2" for an open water system. Which one should I choose?
  • Can I mount an EV220B valve upside down?
  • I have mounted an EV220B valve in the warm water circuit of a heating system. The valve does not open. Is it defect?
  • I have ordered an EV220B valve NO, but if I blow through the valve, it is closed. Have I got a NC valve?
  • Why is an EV220B solenoid valve more expensive than an EV220A valve?
  • How can I replace 032U7328?
  • I assemble air suspension system for cars, does Danfoss have any solenoid valve for this kind of application?
  • What is the difference between the EV220B and EV250B valves?
  • Is it possible to install an EV220B (15-50 series) on vertical pipes?
  • Does Danfoss offer a solenoid valve KIWA approval, neccasary to approve a water pump module?
  • Which solenoid valve should I choose for Glycol as a medium?
  • I have an EV220B 25B that does not close properly - should I unscrew the equalising orifice to close it?
  • Which solenoid valve should I choose for showers?
  • Which coil type fits the EV220B valve?
  • Can I get Danfoss solenoid valves suitable for seawater?
  • Can I an EV220B valve for vacuum?
  • In a open water system, I have an EV210 valve which does not open - what can be wrong?
  • Are your valves certificied for use with water?