>
My Product List
Categories
>
Refrigeration and A/C
Thermostatic Expansion Valves
Solenoid Valves
Pressure and Temperature Regulators
Electronic Controls
Line Components
Pressure Controls and Thermostats
Water Valves
Filter Driers and Sight Glasses
Contactors & Motor Starters
Electronic Controls: Sensors, Transmitters
Electronically Operated Valves
Stop and Regulating Valves
Safety Valves
Liquid Level Controls
Condensing Units
Appliance Controls
Controls Accessories and Spare Parts
Compressors
ICF, Industrial Refrigeration Control Solutions
>
VLT® Drives
Frequency Converters
Decentral Products
Soft Starters
Power Options
>
Industrial Automation
Solenoid valves
Coils for valves
Pneumatically operated valves
Thermostatic valves
Pressure transmitters
Pressure switches
Pressure switches, differential
Temperature sensors
Temperature switches
Temperature switches, differential
Electronic soft starters
Contactors and Motor Starters
Accessories and Spare Parts
>
Heating
Thermostatic Radiator Valves
Time Controls
Electric and Electronic Room Thermostats
Underfloor Heating
Motorised Control Valves
Balancing Valves
Solar Heating Regulator
Bathroom Accessories
>
High-Pressure Pumps
Valves
Pumps
Motors
Nozzles
Powerpacks
About Us
Aspiration, Promise, Behaviour
Danfoss in the UK
Related Companies
Products
Categories
Business Areas
Refrigeration and Air Conditioning
Heating
Industrial Automation
VLT
®
Drives
High-Pressure Pumps
News & Events
News
Newsletters
Archive
Global News Magazine
Jobs & Careers
Danfoss in the UK
Worldwide
Contact
Danfoss in the UK
Worldwide
E-Business
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
Print Page
>
Home
>
Products
>
Categories
>
Pressure switches
>
KP, Dual pressure switches
KP, Dual pressure switches
Danfoss dual pressure switch type KP 44 is designed for use as a pump guard to control and protect supply water pumps. It combines the functions of a pressure switch and a flow monitoring device. The...
>
Code number selector
>
Photos (2)
>
FAQ (14)
>
Approvals & certificates (8)
>
Literature (11)
>
Contact
14 Item(s)
FAQ
What is the maximum/minimum pressure/temperature at which Danfoss switches can be set?
Answer: Danfoss manufactures various pressure switches which can have a setting range of anywhere between -1 to 400 bar and temperature switches from -60 to +300°C. However, each switch will have its own regulation range as detailed within the product catalogue pages. It is always good practice to avoid choosing a product which will be switching near to the limits of its range.
What is the DIN numbering of terminals?
Answer: Terminal numbers are always ODD for inputs & EVEN for outputs, which explains why the changeover switch in almost all pressure & temperature switches has numbers 1, 2 & 4. The live feed goes in at 1. It comes out at 2 when the pressure or temperature is low (so take this to your pump or heater as a live feed) out of 4 when the temperature or pressure is high. (You can take terminal 4 to a ''satisfied'' tell-tale lamp or to an unloading valve or cooling fan, if you wish).
After installing the switch and making the setting based on scale values, the real system pressure value and scale value seem not to correspond. What is the reason?
Answer: Scale values are indicative only and for accurate settings a pressure gauge (for pressure switches) or a thermometer (for temperature switches) must be used.
I am looking for the on/off switch with the highest possible IP protection, what options do I have?
Answer: KPS and CAS pressure and temperature switches has the highest IP protection - IP67.
How does the manual reset work in relation to on/off switches?
Answer: After cut out operation, the unit (pressure or temperature switch) will not cut in until the reset button is manually activated.
What does SPDT stands for?
Answer: Single Pole Double Throw refers to the type of the contact system.
What is the most common contact system type used in Danfoss switches?
Answer: The SPDT (Single Pole Double Throw) contact system is the most used.
Is it possible to improve the IP enclosure grade for KP switches?
Answer: Yes, it can be upgraded to IP55 - using the transparent or non-transparent enclosure (both sold as accessories).
What would be the best pressure switch choice for applications requiring high repeatability, accuracy and adjustable differential?
Answer: RT switches used for regulation, monitoring and alarm purposes feature the highest repeatability and accuracy. They are also available with adjustable differential.
When is it recommended to use a gold-plated contact system?
Answer: Gold plated contacts are particulary suitable for low voltage contol systems.
Where I can find technical information regarding on/off switches?
Answer: In our internet catalogue you can see all relevant product data, as well as download literature and approvals for the specific products.
How many cycles can KP switches perform?
Answer: Units are taken from current production for life tests, electrical and mechanical. The tests are carried out under the most severe conditions. The mechanical life time test has to fulfill at least 400,000 cycles – the average is 1,000,000 cycles. The electrical life time test has to fulfill at least 100,000 cycles (under full load) – the average is 400,000 cycles.
Which switches should I use for seawater - or other media with particles or depositions?
Answer: In case of seawater you should generally use diaphragm versions of switches: - KPS 43, 45 & 47 - CAS 143, 145 & 147 - MBC 5100 with diaphragms Seawater may contain contamination and certainly salt, both of which will likely accumulate inside the application. Not least inside the switch,, because the water inside is almost still (no flow). If salt crystallizes on the bellows surface it can easily affect its proper function. In case of diaphragms, very smooth and flexible, this problem is less visible. This will cause the depositions to be removed from its surface, and until the whole system is filled and blocked with depositions, it will work. Depositions are especially dangerous when you have a small bellows - like in MBCs. If you need to use bellows version of switches then try to choose comparatively big bellows - surfaces on which depositions are stored are comparatively far away and it would take a longer time before they affect bellows function. RT is a switch of this kind.
Where do I find production date on pressure or temperature switches?
Answer: Look for a code similar to the below: AB - identifies factory location (in this case, Poland) 29 - first two digits tell you production week 6 - last digit tells you about production year (2006)