Categories
> Refrigeration and A/C
> VLT® Drives
> Industrial Automation
> Heating
> High-Pressure Pumps
 
 
 
 
 

MCI, CI-tronic™ soft starters

18 Item(s)

FAQ

  • What is special about the MCI Compressor Starter? Can I use a “normal” MCI soft starter to soft start a compressor?
  • Can the MCI soft starter be used as a switch or do I need also to install a contactor?
  • Why does the MCI soft starter only control 2 of the 3 phases?
  • Why do the MCI 15 and MCI 25 not feature integrated by-pass of semiconductors?
  • What does “automatic detection of missing phases” mean?
  • Do you have a soft motor starter for 100 HP?
  • I have mounted a Softstarter MCI C on my air compressor - why doesn't it work?
  • How do I select the correct soft starter?
  • Do soft starters have any internal protection?
  • What is maximum overload current of soft starters?
  • I have a 21 kW motor application with star-delta starter, how can I change to softstarter in the cheapest way?
  • What is trip class?
  • What is the difference between MCI xx and MCI xx C families?
  • Why do we bypass the soft starter in steady state?
  • Does the MCI-CH have some protection against phase change?
  • How should I interpret MCI rating index AC-53b?
  • How should I interpret MCI rating index AC-53a?
  • What does AC-53a and AC-53b stands for and what is a difference?