News
> Business
> Products
> Events & Shows
> Global news magazine
 
 
 
 
 
Danfoss Logo
Legoland

VLT® drives control energy consumption at LEGOLAND® - saving energy with a splash

07 June 2012
190,000 kWh of electricity saved per season by installing Danfoss VLT® drives on the Vikings River Splash attraction at LEGOLAND®

The popular Vikings River Splash in LEGOLAND® consumes more energy than nearly everything else in the amusement park.

After installing two 132 kW, VLT® 6172 frequency converters to control the pumps that ensure a stable and reliable flow of water, the attraction's energy consumption has dropped from 440,000 to 250,000 kWh per season.

At the same time LEGOLAND® has been able to increase the number of boats they can send off filled with fun seeking guests.

Legoland