(UK) Danfoss United Kingdom
News
> Business
> Products
> Events & Shows
> Global news magazine
 
 
 
 
 
Danfoss Logo
VLT Micro Drive FC 51

VLT Micro Drive 18,5 and 22 kW now available

19 August 2009
The power range of the VLT Micro Drive FC 51 has been extended with two new ranges; 18,5 kW and  22 kW.

Production of the new drives has started and orders are accepted as from today. Deliveries will start by week 36.
The VLT Micro Drive FC 51 is a general purpose drive that can now control AC motors up to 22 kW. It is a small drive with maximum strength and reliability. This makes the VLT Micro Drive the perfect match for industrial and HVAC OEM-applications.

The VLT Micro Drive is manufactured with respect for the environment, and it complies with the RoHS Directive.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.