News
> Business
> Products
> Events & Shows
> Global news magazine
 
 
 
 
 
Danfoss Logo
Coolselector

Coolselector®: Cool Releases

15 June 2012
Our successful selection tool Coolselector® has been updated today!

If it is already installed on your computer you will be prompted to update Coolselector® the next time you are using it whilst connected to the internet. If you do not already have it installed why are you missing out? Download it via the link below! 

The update means that Coolselector® now also includes the latest models of compressors and condensing units. Among the other updates in the new release is the addition of the latest Optyma Plus New Generation condensing units.
The new version also offers the selection of electronic controls divided up into Pack Controls, Evaporator Controls, System Controls, Accessories and Frequency Converters

Coolselector® version 1.0.1.2 has also got improved calculations of several control valves such as thermostatic expansion valves, solenoid valves and other controls.

Do not miss out on all of these great new features - version 1.0.1.2 of Coolselector® is now available for download via the link below

Coolselector® is quite popular among many of our customers and is used worldwide, translated into 12 languages and has thereby become a great success for Danfoss. If you have not already got the software installed please visit our Coolselector® website today and download it. It is free for use both for individual users and for corporate distribution purposes.
KoolApp - CoolGame

KoolApp™ CoolGame - Can You Take On The World?

Test your refrigeration know-how compared to colleagues around the world. Establish your own league against you colleagues or classmates or play against the world!

The gaming concept is that you build a specific refrigeration circuit as fast as possible by placing the components in the correct place in the system.