Refrigeration and Air Conditioning
> News
> Newsletters
> Products
> Technical Literature
> Software
> Refrigeration Scroll
> OPTYMA PLUS™ Condensing Units
> Optyma Plus™ New Generation
> Heat Pump Performer®
> ICV
> Telecom Cooling
> Mobile Refrigeration
> One Reason - Many Savings
> Refrigerants
> The Industries We Serve
> Training & Education
> Subscribe to Cooling Matters
> About Us
> Contact Us
> Distributor Network
 
 
 
 
 
Danfoss Logo
Pressure Regulators

Fitters Notes Series: Pressure Regulators

10 September 2008
Pressure regulators are necessary to regulate the pressure of certain components of the system. For example, an evaporating pressure regulator defines a certain minimum pressure in an evaporator, while a condensing pressure regulator does the same thing for a condenser. A crankcase pressure regulator prevents the system from exceeding a defined setpoint pressure, and a capacity regulator, which is also called a hot-gas bypass regulator, mixes in hot gas if the pressure on the low-pressure side drops below the setpoint pressure level. The purpose of a receiver pressure regulator is to initially bypass the condenser during system start-up in cold weather, after which it closes the bypass when a stable operating state is achieved.

Useful practical tips for the everyday work of fitters is provided in the “Fitters Notes” series. The “Fitters Notes” series is based on the handbook of the same name produced by Danfoss, which discusses the basic principles of commercial refrigeration systems and the associated basic components.
Click below to download the story as .pdf or go to our online article overview.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.