Refrigeration and Air Conditioning
> News
> Newsletters
> Products
> Technical Literature
> Software
> Refrigeration Scroll
> OPTYMA PLUS™ Condensing Units
> Optyma Plus™ New Generation
> Heat Pump Performer®
> ICV
> Telecom Cooling
> Mobile Refrigeration
> One Reason - Many Savings
> Refrigerants
> The Industries We Serve
> Training & Education
> Subscribe to Cooling Matters
> About Us
> Contact Us
> Distributor Network
 
 
 
 
 
Danfoss Logo
Pressure Controls

Fitters Notes Series: Pressure Controls

22 September 2008
The actual pressure in the system at the point monitored by the pressure control is usually provided via a branch line or – if the pressure control is installed directly on a line – applied directly to the pressostat. The pressure actuates a potential-free set of contacts that can be used to control a device such as a compressor or a fan.

Useful practical tips for the everyday work of fitters is provided in the “Fitters Notes” series. The “Fitters Notes” series is based on the handbook of the same name produced by Danfoss, which discusses the basic principles of commercial refrigeration systems and the associated basic components.
Click below to download the story as .pdf or go to our online article overview.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.