>
My Product List
Industrial Automation
>
Product information
Products for industrial applications
Solenoid Valves
Thermostatic Valves
Angle seat valves
Pressure Transmitters
Pressure Switches
Temperature Sensors
Temperature Switches
Industrial heat exchangers
Bio-mass valves
>
News
>
News Archive
>
Documentation
Literature
Approvals & Certificates
>
Distributors
>
Contact Us
>
Technical Support
FAQs
Quick Service Request
About Us
Aspiration, Promise, Behaviour
Danfoss in the UK
Related Companies
Products
Categories
Business Areas
Refrigeration and Air Conditioning
Heating
Industrial Automation
VLT
®
Drives
High-Pressure Pumps
News & Events
News
Newsletters
Archive
Global News Magazine
Jobs & Careers
Danfoss in the UK
Worldwide
Contact
Danfoss in the UK
Worldwide
E-Business
Local Sites
Danfoss Group Global
Afghanistan
Argentina
Australia
Austria
Bahrain
Belarus
Belgium (Dutch)
Belgium (French)
Bolivia
Bosnia - Herzegovina
Brazil
Bulgaria
Canada
Chile
China
Colombia
Costa Rica
Croatia
Cuba
Czech Republic
Denmark
Djibouti
Dominican Republic
Ecuador
Egypt
El Salvador
Eritrea
Estonia
Ethiopia
Finland
France
Germany
Guatamala
Haiti
Hungary
Iceland
India
Indonesia
Iran
Ireland
Italy
Jamaica
Jordan
Kazakhstan
Korea
Kuwait
Laos
Latvia
Lebanon
Lithuania
Malaysia
Mexico
Middle East
Netherlands
New Zealand
Norway
Oman
Pakistan
Paraguay
Peru
Philippines
Poland
Portugal
Puerto Rico
Qatar
Romania
Russia
Saudi Arabia
Serbia
Singapore
Slovakia
Slovenia
Somalia
South Africa
Spain
Sudan
Sweden
Switzerland (French)
Switzerland (German)
Syria
Taiwan
Thailand
Turkey
Ukraine
United Arab Emirates
United Kingdom
United States of America
Uruguay
Venezuela
Vietnam
Yemen
>
Print Page
>
Home
>
Business Areas
>
Industrial Automation
>
Products
>
Fluid Control
>
Thermostatic valves
>
WVTS, Thermostatic valves with temperature sensitive sensor
WVTS, Thermostatic valves with temperature sensitive sensor
Cooling water valves of type WVTS are suitable for controlling the temperature of a flow of water or neutral brine.WVTS opens on rising sensor temperature. Large self-acting cooling water valves for...
>
Code number selector
>
Photos (2)
>
FAQ (13)
>
Literature (9)
>
Contact
13 Item(s)
FAQ
What does it mean that thermostatic valves are proportional and self-acting?
Answer: Proportional means that on sensor temperature change, the cooling water flow quantity change is proportional. This correlation is kept up to 85% of valve capacity. Self-acting means that thermostatic valves operate without the supply of external auxiliary energy such as electricity or compressed air. It is a very important advantage of thermostatic valves because even at breakdowns in the power supply, the valve will still function, e.g. keep cooling the application.
Is it possible to replace a copper capillary tube with a stainless steel version?
Answer: No, unfortunately elements with stainless steel capillary tube are not available, but we recommend using a thermostatic element with stainless steel armour, protecting the capillary tube's entire length.
What is off-set for thermostatic valves?
Answer: It is the temperature on sensor that corresponds to 85% of valve opening. Above that number, the link between controlled temperature and water flow is no longer linear and temperature control is less precise.
Is there any temperature range preset made for the WVTS valve?
Answer: No, there is no preset done in the factory for WVTS valve. You have to adjust the element to meet your demand for opening temperature.
Can you send me a 3.1 certificate for a valve already delivered?
Answer: The inspection certificate 3.1 involves test results that shall be carried out during production process for the specific valve. For valves already produced, we are therefore not able to issue this certificate. Therefore, when ordering, please specify the need for the certificate.
Permissible working pressure for the WVTS valve is 10 bar. What will happen if WVTS will be installed in application where pressure is maximum 16 bar?
Answer: If the pressure is higher than the allowed, it is likely that the permanent influence shortens the life period of the internal parts of the WVTS valve. In such cases, we recommend using 2 AVTA valves in parallel connection instead of one WVTS. The AVTA can operate at 16 bar and thus be used without problems.
The pilot unit for WVTS valve is supplied with white plastic washer - is it only packaging protection to be thrown out?
Answer: The white plastic washer is essential part of the valve – without this component, WVTS loses its functionality. Please remember to check presence of this part during assembly of pilot unit and WVTS valve body.
Is it necessary to install a filter ahead of thermostatic valves?
Answer: We always recommend installing a filter type FV in the pipe system ahead of valves, especially in cases when the medium could be contaminated or include dirt particles. A dirt filter should be always installed ahead of the FJVA valve, which has a small-diameter bypass in the valve body.
Are AVTA, FJVA and WVTS valves UL or CSA approved?
Answer: No, they are not approved as they don''t have any electrical components, and therefore an approval is not needed.
My WVTS 80 valve has 8 holes for flange connections, but the technical brochure shows only 4. Is the product wrong?
Answer: WVTS sizes 50 and 65 have 4 holes for flange connections. Bigger valves WVTS 80 and 100 are fitted with 8 holes.
For thermostaticall operated valves, are there any requirements to the cooling water temperature?
Answer: The only requirement is that the cooling water temperature should be less or equal to the setting temperature. If the cooling water temperature is close to that point, then more capacity is necessary to cool down the process medium. We may in this case recommend a bigger valve size than in cases when the cooling water temperature is lower. How to select proper size of the valve depending on cooling water temperature is shown in the data sheet.
Is it possible to order a WVTS valve with other charge than universal?
Answer: No, WVTS is available only with universal charge.
Are thermostatic valves AVTA, FJVA, WVTS normally closed or normally open valves?
Answer: Thermostatic valves valves are NC - normally closed. They open on rising application temperature.