Oil-free compressors
1 million tons of CO2 are saved every year through the Danfoss Turbocor compressors that are installed in commercial buildings worldwide. Today, far less than 1% of commercial buildings have indoor climate systems with oil-free, variable speed compressors. The potential is huge. In the US alone, 950 million tons of CO2 could be saved every year, if all commercial buildings had systems with this kind of compressor1.