News
> News stories
> Case stories
> Opinions
> Subscribe Solutions Ready Newsletter
> RSS News Feeds
> A Bright Green weekend of solutions, dialogue & learning
 
 
 
Danfoss Logo

One-pipe heating costs cut in half

January 30, 2012
Pilot test in Russia proves that renovation projects can make old one-pipe heating systems as energy-efficient as two pipe systems. The buildings in the test became 45 percent more energy-efficient.
The tenants in two Moscow apartment buildings from the 1960s no longer have to open their windows if their apartment gets too warm during winter. They simply adjust the Danfoss thermostats installed in each room to get the temperature they want.
 
The thermostats are just some of the components installed as part of a comprehensive modernization project Danfoss has taken part in along with the local company in charge of administration and service of the buildings.

The project shows that it is relatively easy to make old one-pipe heating systems up to 45 % more energy efficient – with a pay-back time of only 3.6 years.

“With this project, we have achieved several important results. First of all, the heat consumption was reduced and the number of complaints from tenants decreased significantly. Second, we now have a new and very reliable system with a high quality of service management,” says Sergey Dzyuba, deputy chief engineer at the local company in charge of service and administration in the buildings.


Bringing one-pipe system back from the grave

But let’s first take a look at the system as it was before Danfoss came into the picture.

One-pipe systems are generally not energy-efficient because hot and cold water share the same return pipe. The apartments were therefore insulated and had new windows installed as part of the Moscow renovation project.

But as the buildings’ old heating system did not leave tenants with the option of controlling the temperature, the apartments often got overheated – even with subzero temperatures outside. The conventional solution would be to install a two-pipe system. And that’s a costly affair.

So the company in charge of administration and service of the buildings opted for a Danfoss proposal to renovate the one-pipe systems instead. The solution included installation of thermostatic radiator valves, automatic balancing valves, and new heating substations with weather compensation in the basements to ensure that heating is automatically adjusted according to the outdoor temperature.

To secure maximum energy-efficiency, Danfoss also equipped the balancing valves with thermostatic sensors. So, when return water temperature exceeds preinstalled settings, the balancing valves automatically reduce flow in the risers.
“In very basic terms, this is how it works. Danfoss is the first company to prove that you can make one-pipe systems so energy-efficient. The solution costs only a fraction of the cost of a full-scale renovation into a two-pipe system,” explains Project Coordinator Maria Zhukova, Danfoss, Poland.

The pilot project was carried out during 2010 and 2011 on three identical buildings in Moscow. Two of the buildings had Danfoss equipment installed; the third was used as a reference building with no extra Danfoss equipment installed.




Pictured right: The one-pipe system after the renovation. The installation of automatic balancing valves AB-QM ensures stability in the system with all risers well-balanced and guarantees that the energy consumption is evenly distributed across the system.
Comments
Wang Weiqiang February 6, 2012
If I understand correctly, The pilot project was carried out during 2010 and 2011, this news should be published ealier.
Camilla Karlsen - Danfoss February 7, 2012
Hi Wang,

It is correct that the pilot was carried out in the winter of 2010 and 2011.

After the period the data were collected from the three buildings, and of course, they had to be studied by the project team who also made the calculations on the final savings.

Because of this we couldn't publish the story earlier.

Best regards,
Camilla Karlsen, Danfoss
floura February 12, 2012
Hi,
Is DCS/DES supplied by Danfoss?
Indonesia i thought really potential market....
None ever used DES DCS in here
thx

Maria February 13, 2012
Hello Floura,

thank you very much for your questions, but would you be so kind to write what is behind the abbreviation DCS/DES?

BR, Maria
maciej April 2, 2012
Why somebody erased my previous post?
M.Roczek
Camilla Karlsen - Danfoss April 2, 2012
Dear Mr. Roczek,
I am afraid I can't find any previous posts from you in our comment system, not even in the trash folder.

I would like to kindly request that you post your comment/question again.

Thanks a lot and have a nice day!

Best regards,
Camilla Karlsen - Danfoss
Your Name:

Your e-mail address will remain undisclosed to others than the site owner

Message:






Solutions Ready

Solutions Ready

Danfoss has 78 years of experience within the field of energy efficiency through optimized utilization of resources.
Our reasoning is very simple: Money saved today is the best foundation for investments in tomorrow's energy saving technologies.