(AU,NZ) Danfoss Pacific
Refrigeration and Air Conditioning
> News
> Products
> Technical Literature
> Software
> The Industries We Serve
> Training and Education Materials
> About Us
> Contact
> Australian and New Zealand Wholesaling Outlets
 
 
 
 
 
Danfoss Logo
Danfoss EnFusion BPHE Calculation Software

Danfoss EnFusion™ Hex Calculation Software

With Danfoss EnFusion™ Hex Calculation Software, you can carry out calculations in design, rating or performance mode of the brazed plate heat exchanger for single phase, condenser and evaporator units.

The usage of the Danfoss Danfoss EnFusion™ Hex Calculation Software requires approval by Danfoss.

After the installation is complete you will have to send us your Application Code in order to receive the Registration Code needed for activation of the software.

Danfoss reserves the right to refuse anyone the usage of this software without explanation.

System Requirements

Operating System
The Danfoss Danfoss EnFusion™ Hex Calculation Software supports the following operating systems: Windows 98, Windows 2000, Windows NT, Windows XP, Vista

Microsoft Office Version
The Danfoss Danfoss EnFusion™ Hex Calculation Software requires Microsoft Office 2000 or higher installed on your PC.

Download Details
The download details for Danfoss EnFusion™ Hex Calculation Software Version 2009.03 are as follows:

1: Please create a new folder on your local drive. e.g. C:\Download Disk
2: Now right click on the Download link below and use the Save Target As.. option and download the .zip file to the folder you just created.
3: After you have downloaded the .zip file, Unzip the disk, in the same folder
(In case you do not have WinZip on your machine you can download it from the site from the WinZip Link below and install it your machine)
4: Go to the unzipped folder and run the Setup Application to install the software.
5: When the installation is complete, run the software. You will be asked to type in the Registration Code, to match the given Application Code.
6: Please copy the application code, and use the mailform below ('Retrieve Registration Code') together with the reference name of your contact in Danfoss. Pending approval of your application code, the connected Registration Code will be sent to you as soon as possible.
7: After you enter the Registration Code, the software will start and the login screen will appear.

Note: If you already registered previous versions of this software from versions higher than 2009.01, you do not need to register again.

Limitations on Vista: There may be limited access to the help files if you are using Vista as your operating system. You cannot view the help files created in Winhelp (Accessed through Start -> Programs -> BPHECalc version 2009.03 -> Help).
However you can access the help inside the Danfoss EnFusion™ Hex Calculation Software by clicking menu Help -> Contents (Since this help is created in HTMLHelp).

Contact Us
You are welcome to contact us should there be any questions or queries, please use the email link below.

DISCLAIMER
All values calculated and selected by this software must be verified by the user. Danfoss can accept no responsibility for possible errors in the Danfoss EnFusion™ Hex Calculation Software. Danfoss reserves the right to alter its product withour prior notice. This applies to products already in order provided that such alterations can be made without subsequential changes being necessary in specifications already agreed. All trademarks in this material are the property of the respective companies. Danfoss and the Danfoss logotype are the trademarks of the Danfoss A/S. All rights reserved. ©2009 Danfoss A/S

Working with you to improve your business

In everything we do our main principle is
to be customer driven to satisfy short and long term customer needs and expectations. Our aim is always to be perceived as being THE BEST CHOICE, PREFERRED PROVIDER and BUSINESS PARTNER.
Together we can improve your business.
So if you want the support of a company that works to improve the efficiency and profits of your business, call us today
We are here to make it happen