7 Item(s)
FAQ
I have bought the valve AV210, can you offer me the pilot valve to do the control?
I have installed an pneumatically operated valve type HP210 and it does not work any longer. Can you offer me a new one?
How can I control air for pneumatically operated valves?
What pressure is required to control AV210 ?
Can I use the AV210 for waste water ?
Answer: Yes, the AV210 has a resistant floating disk that gives a secure sealing on the orifice.
This is also benefitial when using steam. Steam can be aggresive and contains impurities, and this valve is good for steam and trouble shooting in general.
I work with steam and the Danfoss solenoid valve EV225B does not have enough flow. Can you recommend another option?
Could the AV210 capacity control be used together with the AV210 position indicator?