News
> News Overview
> Business & Finance
> Products
> Events & Shows
> Global news magazine
> RSS News Feeds
 
 
 
 
 
Danfoss Logo

Danfoss Introduces Brazed Plate Heat Exchangers

22 January 2008
Danfoss, a global leader in supplying components, controls, compressors and solutions for air conditioning and refrigeration, has introduced the newest extension of its product portfolio, brazed plate heat exchangers.
Danfoss brazed plate heat exchangers are tailored for refrigeration and air conditioning systems, can be customized for specific application requirements, and offer an environmentally responsible solution for a wide range of applications. Each brazed plate heat exchanger is engineered to add value over its lifetime, providing superior performance and cost-effectiveness.

Each brazed plate heat exchanger consists of a series of thin, corrugated stainless-steel plates that are brazed together in a vacuum furnace, resulting in a rugged and highly efficient heat exchanger. Plates are stacked, turning each plate 180º to create two flow channels that induce a high degree of turbulence, which increases thermal efficiency while maintaining low pressure drop. Danfoss brazed plate heat exchangers can accommodate gas or liquid media.

“We are continuously striving to develop and provide environmentally friendly and energy-efficient products,” says Peter J. D’Ambrosio, strategic global marketing manager-heat transfer, Danfoss Inc. “Our brazed plate heat exchangers are space-saving, offer a highly flexible design for manufacturing, and require less use of refrigerants.”

“With our entire range of heat exchangers, we offer our customers an opportunity to define both the capacity and connections they need for their specific application,” D’Ambrosio says. “As an added benefit to the customization options, the brazed plate heat exchangers, because of their high heat transfer performance, contribute to an increase in overall cooling capacity. This not only reduces energy consumption, but it provides the best value over the longest period of time as well.”

Danfoss offers 15 brazed plate heat exchanger models. Each model is compactly designed and combines high efficiency with energy-saving qualities.

Model B3-048 is designed with a special patent of different corrugation depth on the same plate. With a capacity of 30 – 80 kW, this model allows a larger water flow rate, lower pressure rate drop and lower refrigerant charge. Model B3-260 is the ideal choice for HVAC and chillers, while Danfoss makes 10 different models for boilers and chillers. And, for air driers and chillers, Danfoss recommends models B3-014, B3-027 and B3-136. The entire range of brazed plate heat exchangers can also be used for heat pumps, economizers, de-superheaters and numerous other applications.

Danfoss brazed plate heat exchangers perfectly fit applications in the food, beverage, pharmaceutical and chemical process industries, in indirect and direct air compressors, and in commercial refrigeration applications such as supermarket systems, ice making machines, beverage, beer cooling and more.

For more information about Danfoss, call (410) 931-8250 or visit www.danfoss.us.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.