News
> News Overview
> Business & Finance
> Products
> Events & Shows
> Global news magazine
> RSS News Feeds
 
 
 
 
 
Danfoss Logo
U.S. Congressman F. Allen Boyd Jr. (second from left) poses in the lobby of Danfoss Turbocor Compressors’ manufacturing facility in Tallahassee, FL, with a Turbocor compressor.  Joining him are (from left) Danfoss employees Lisa Tryson, director of branding, Americas; Ron Conry, founder of Danfoss Turbocor; and Dan Thatcher, vice president, aftermarket sales and marketing, Danfoss Turbocor.

Making a Case for Advanced, Oil-free Compressor Technology

16 July 2009
U.S. Congressman Visits Danfoss Turbocor Manufacturing Facility
If a prominent U.S. congressman has anything to say about it, Danfoss Turbocor’s advanced compressor technology will have a much larger stake in federal, state and commercial facilities in the U.S. That’s because the technology makes air conditioning equipment more efficient, significantly reduces energy consumption and creates “green” jobs in the HVAC industry.

“The private sector will play a significant role in our national energy policy as our country begins to move toward energy independence,” said Congressman F. Allen Boyd Jr. (D-Fla.), who recently toured the Danfoss Turbocor Compressors manufacturing facility in Tallahassee, FL. “This visit was a great opportunity to learn more about the important work being done right here in North Florida to advance the latest energy technologies. New energy-efficient technologies, like those being developed at Danfoss Turbocor, are a key component of reducing our energy consumption and energy costs.”

Boyd’s district includes the Tallahassee area, where he has served as a congressman since 1997. He is a member of the House Budget and Appropriations Committee.

Ricardo Schneider, president and CEO of Danfoss Turbocor, complimented the congressman on the timing of his visit. “The economic stimulus package can have a huge impact on federal, state and commercial facilities in the U.S.,” Schneider said. “Working with the administration under the stimulus program presents a unique and significant opportunity for Danfoss Turbocor to help the HVAC industry become more energy efficient and environmentally sustainable.”

Meeting Industry’s Needs for Future
To date, over 14,000 Turbocor compressors are in operation worldwide. The current installed base of those compressors is reducing CO2 emissions by over 4.4 million tons/year, which is equivalent to removing approximately 600,000 passenger cars from roadways.

Several Original Equipment Manufacturers have incorporated the technology into their chiller systems. They include:

  • McQuay created the world’s first AHRI-certified frictionless chiller using the Danfoss compressor. With a capacity of up to 300 tons of refrigeration (TR), the chiller has a full-load value as low as .575 kW/ton and an Integrated Part Load Value (IPLV) of .375 kW/ton. The chiller uses environmentally friendly R-134a refrigerant and has a sound rating of only 77 dba.
  • Multistack uses the Danfoss technology in its modular chillers and high-efficiency MagLev™ chillers. The modular chillers are energy efficient, compact and quiet, while the MagLev chillers range from 120 to 600 TR, use R-134a refrigerant, require only 2 amps in rush current, are quiet and have an IPLV of .38 kW/ton. In fact, the U.S. Mission to the United Nations officially launched its new 225-ton MagLev chiller on Earth Day 2009 at a meeting in Geneva, Switzerland.

The technology has won numerous awards in the past 10 years, including the U.S. Green Building Council’s LEED certification (2007), U.S. EPA Climate Protection Award (2004), ASHRAE/AHR Expo Energy Innovation Award (2003), Canada Energy Award (2004) and Frost Sullivan Award for HVAC Innovation (2006).
According to Ron Conry, who invented the technology 15 years ago, it’s truly transformational because it features magnetic bearings, which use 99.5 percent less energy compared to conventional bearings. The magnetic bearings are key to the compressor’s oil-free design, he added.

Conry noted that the technology is already being used in some federal buildings and U.S. naval stations, including the San Diego facility. The Navy’s Technology Validation Program recently yielded nearly 10,000 tons of Danfoss Turbocor compressors.

“We’re just scratching the surface when it comes to adopting this technology in the U.S.,” Conry said. “More and more facility owners and managers are beginning to recognize its benefits. As governments around the world promote energy and environmental concerns, building owners are coming to realize that efficiency and life cycle costs are what the future is about, and although first cost is an important consideration, it does not reflect the real cost of ownership. Fortunately for us, we happen to have the right technology at the right time.”

On the commercial side, NFL Films in Mount Laurel, NJ, uses the technology in Smardt chillers to cool its 200,000 square-foot studio complex, which houses the world’s largest sports film library. The technology has enabled NFL Films to reduce its electricity consumption by 10-12 percent – from 11 million kilowatt-hours (kWh) per year to under 10 million kWh.

A History Worth Noting
In 1994, Conry invented a compressor that would meet the industry’s needs for the future, based on his own extensive experience in the field of chiller and compressor rebuilding and maintenance. He assembled a world-class international team of experts with a mission to develop a centrifugal compressor that would operate at high variable speeds, be extremely efficient, oil free, lightweight, quiet and cost competitive. In order to commercialize the compressor, in 2004 Turbocor entered into a joint venture with Danfoss and formed Danfoss Turbocor Compressors Inc.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.