News
> Business & Finance
> Products
> Events & Shows
> Refrigeration News
> Drives News
> Industrial Automation News
> Heating News
> Solar Energy News
> Global news magazine
> RSS News Feeds

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

VLT® low voltage drive replaces expensive high voltage drive

15 July 2009
A standard low voltage VLT® drive has successfully replaced an expensive medium voltage drive in an Indonesian crude oil deep well pump-application and delivers great performance with respect to the required throughput and pump protection.
By adjusting the pump speed, it is now possible to extract crude from the well without rapid depletion, thereby optimizing the production and prolonging the application life time.
A standard low voltage (LV) drive offers a cost-effective alternative to its medium voltage (MV) counterpart when configured in a HI-LO-HI type power configuration. There are numerous advantages in using a VLT® drive in this configuration:

• The design represents a high degree of user friendliness by virtue of using standard components and proven low-voltage IGBT technology.

• It retains the existing ac motor, eliminates voltage reflections, common mode voltages and potentially harmful bearing currents, thereby prolonging the life of the motor. This is made possible by the use of a sine filter which delivers a sinusoidal voltage at the motor terminals. The solution is therefore motor friendly.

• Derating of the drive motor for inverter operation is not necessary, since the motor sees a sinusoidal voltage at its terminals and losses remain the same as for operation from a fixed frequency mains supply.

• The user has the advantage of stocking standard spares and thereby reduces inventory costs.

• Existing users of VLT® drives need not undergo retraining to assimilate new technology, which would be the case with a direct MV Drive. Hence the system saves on training costs.

The solution was put into practice at an application involving an electric submersible pump (ESP) for crude oil extraction from an underground oil well. Sinar Surya Graha Persada, a sub-contractor for Pertamina Corporation, a state owned Petroleum Company located in Jambi province of Sumatra, Indonesia, decided to use the Danfoss solution. This involved replacement of an existing MV Drive with a VLT ® Automation Drive which was engineered in a LO-HI configuration.

Some key reasons for choosing Danfoss, included:

• Its vast experience of supplying drives for critical applications.

• Positive feedback from other customers regarding the performance of VLT® Automation Drive

• Its ability to provide quality application know-how, and service at short notice.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.
Feedback Form