News
> Business & Finance
> Products
> Events & Shows
> Refrigeration News
> Drives News
> Industrial Automation News
> Heating News
> Solar Energy News
> Global news magazine
> RSS News Feeds

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

The New VLT® MCD 500 Soft Starter

21 January 2009
– The single speed drive  

Danfoss’ new VLT® MCD 500 Soft Starter is a complete motor starting solution with advanced start, stop and protection features, Adaptive Acceleration Control (AAC), built-in delta connections, a four-line graphical display and multiple programming setup menus.
The VLT® MCD 500 is an advanced intelligent motor starting solution that constantly monitors the behaviour of its load to adjust and refine its dynamic performance.

The AAC principle automatically selects and adjusts the best starting and stopping profile for the application. It measures motor current and provides feedback for constant improvement of the motor ramp profiles.  

The MCD 500 offers a four-line graphical display and a logic keypad making programming easy. A more advanced setup is also possible, displaying full operational status. The MCD 500 has three menu systems providing the optimum programming approach: 

             -       Quick Menu, 
             -       Application Setup      
             -       Main Menu

The MCD 500 covers the range 21 – 1600 A. (7.5 – 800 kW), and offers versions for the whole voltage range 200 – 690 VAC.  The power range can be extended to 1.2 MW when using the inside delta connection.

Communication
VLT® MCD 500 Soft Starter has a series of options for serial communication:
            –          DeviceNet 
            –          Profibus 
            –          Modbus RTU 
            –          USB

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.