News
> Business & Finance
> Products
> Events & Shows
> Refrigeration News
> Drives News
> Industrial Automation News
> Heating News
> Solar Energy News
> Global news magazine
> RSS News Feeds

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo
Plug-in Valve

New Plug-in Valve all set for new Types of Refrigerants

28 May 2009
Danfoss has developed a new type of solenoid valve for oil injection in the harsh environment found in a new variable speed refrigeration compressor which uses a new type of refrigerant.

EV219A valve ensures safe injection of oil

Three years ago, Danfoss started to develop the world’s first commercial variable speed scroll compressor for air conditioning using the refrigerant R-410A. In 2006 this refrigerant was relatively new and Danfoss set out to develop a new plug-in valve to ensure safe injection of oil into the compressor to lubricate moving parts.

Two years later, in 2008 the product was introduced to the US market under the name Apexx VSH series. VSH compressors offer greater comfort as a result of tighter temperature control and the ability to cool or heat rapidly on demand by instantly increasing speed. There is significant noise reduction, particularly at part-load conditions, and the Danfoss VSH compressor can exceed 20% in energy savings compared to conventional systems. 
Schroll compressors
In a scroll compressor, oil is mixed with refrigerants, so the task was to make a valve that could withstand this harsh environment. The team of developers tested and chose a special mix in the rubber for the sealing and this made all the difference.
The EV219A plug-in valve performs with this fluid mixture.

The EV219A valve is not only intended for compressor applications, but can be built into every valve housing which needs an actuator. Danfoss can produce value-added designs for a wide range of applications including refrigerant.  

For the US market, Danfoss has acquired an UL-approval for the valve EV219A.  



By Morten Jensen, Lead Design Engineer
Industrial Automation Products

Industrial Automation product catalogue

Dive into our product catalogue and find details about our industrial products:

Read more about our industrial products and applications:
Feedback Form