News
> Business & Finance
> Products
> Events & Shows
> Refrigeration News
> Drives News
> Industrial Automation News
> Heating News
> Solar Energy News
> Global news magazine
> RSS News Feeds

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

New Generation of Danfoss ADAP-KOOL® Injection System for CO2 Evaporators

01 March 2010
Danfoss presents a new generation of ADAP-KOOL® Injection System for CO2 evaporators. The system consists of:
  • Electronic controller AK-CC 550A
  • Electronic expansion valve AKVH
  • Pressure transducers and temperature sensors

The system has a number of innovative features that facilitate the use of CO2, and the exploitation of the full potential of the refrigerant.
One of the CO2 challenges is sudden superheat change, especially in evaporators not fully adapted for CO2. It requires a very fast reaction from the controller. AK-CC 550A electronic controller includes an algorithm for this specific purpose.

Another CO2 challenge is high pressure at standstill position and in some cases high differential pressure over expansion valves for high temperature cases. AKVH valves copes with both tasks. The valves have a MWP of 90 Bar and maximum pressure differential up to 35 Bar! Extremely fast reaction time is another important feature of AKV valves when compared to other expansion technologies.

New Danfoss injection makes it easier to design and commission CO2 systems, thus bringing CO2 faster to the market.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.