Reduce line current by up to 40% with the VLT® Line Filter MCC 107
06 October 2011
The VLT® Line Filter MCC 107 improves drive lifetime and overall reliability by combining a harmonic filter and an EMC filter.
The VLT® Line Filter MCC 107 improves the overall frequency performance of the line current to the VLT® Micro Drive, and offers outstanding EMC performance in the micro-inverter class, even with relatively long motor cables.
By reducing the voltage ripple on the DC link, drive reliability increases and extends the lifetime expectancy of the drive, thereby reducing operation and maintenance costs.