News
> News Overview
> Corporate press releases
> Business & Finance
> Products
> Events & Shows
> Refrigeration News
> Drives News
> Industrial Automation News
> Heating News
> Solar Energy News
> Global news magazine
> RSS News Feeds

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo
VLT® FCD 302

VLT® FCD 302 Decentral Drive now available with pluggable Profinet

22 December 2011
The drive that was introduced at the 2011 Brau Beviale exhibition in a new 3 kW version has been upgraded for easier networking.

The latest upgrade enables customers to choose from a more complete fieldbus portfolio, which now features pluggable Profinet connectivity in addition to Ethernet/IP and Profinet.   Now it is easier than ever to install and connect the drives to the existing network. Where it previously necessary to enlist specialist help to open the drive and draw internal cables, Profinet connectivity is solved simply by plugging in the cables to the drive’s external connectors. 

Install with ease

For owners this saves time in installation and reduces the risk of error. Due to the fact that the drive does not need to be opened, non technical staff can handle the task in only a short space of time.  

The new 3kW drive shares the compact design and easy installation with the FCD 302 series up to 2.2 kW. For optimal installation the drive has retained its flat shape for easy attachment to standard conveyors. The only difference is that it is slightly longer.  

Flexibility remains the same, as the FCD 302 supports standard asynchronous and PM motors for supreme control. Users are free to choose their own motor and manufacturer.

News & Events

Internal and external communication is one of the most important tools we have to help us achieve Danfoss' overall targets, activities and results.
Communication is based on an open and honest dialogue with all stakeholders, which will further their understanding of the Danfoss Group.